Hi Athieshkumar T,
Here is what we use for the TINA reference design: https://www.ti.com/product/AMC1301-Q1#design-development##design-tools-simulation
You can see that there is a working voltage of 500V implemented between the two grounds,…
Hi Kuan,
I have given you lots of circuits to change the output signal of AMC1301 from differential to single ended. And as the output of AMC1301 is already differential, there is no need to convert it from single ended back to differential.
Kuan…
Thanks for your support.
Yes, currently, the VinP is connected to GND_ISO in the board (using 0-ohms R113);
Regarding the part usage in the given low side current-sense circuit;
is there any issue in using the AMC1301 with same GND and Supply…
Part Number: AMC1301 Hi Team,
I want to realize the system such a shunt solution using AMC1301.
Is it possible to output analog signal from 0.5 to 4V when the current which through the shunt resistor is from -2000A to 2000A?
In my understanding…
Part Number: AMC1301 Hi team,
I have a question about the gain of AMC1301. I'm testing the AMC1301 and there are unclear points that are not mentioned in the datasheet. We tested the parts individually, and measured the gain from the relationship between…
Hi Karthik,
I can't give you specific details on what's inside the AMC1301-Q1, but if you take a look at one of our isolated modulators, like the AMC1304 for example, you see what happens through the input modulator stage of the AMC1301-Q1. The modulators…
Part Number: AMC1301 Dear colleague,
A customer prepares to use AMC1301 in digital AC/DC to measure bus voltage.
My customer asked me if exceeded AMC1301 CMTI, what will happen in AMC1301 output?
Do we have a related application note to explain…
Part Number: AMC1301 Other Parts Discussed in Thread: TIDA-01513 , AMC1300 , AMC3330 , AMC1350 , Hi team,
I help my customer to post a question.
"I want to get some technical assist for TIDA-01513 High voltage measurement,in this circuit i think GNDi…
Part Number: AMC1301-Q1
Hello,
In figure 13 ( http://www.ti.com.cn/cn/lit/ug/tidudj6/tidudj6.pdf ) is GNDi common with HV_NEG? This question is rooted in my lack of knowledge in opamps with respect to grounding. Do single-ended, fully differential…