Part Number: AMC1350 Hi Team,
our requirement is to measure 2Vac and we need o/p single ended with isolation
We did simulation with AMC1350. the o/p we wanted is , it ishould be 2.5V ref. but we are not able to get this. can you pl., support.
…
Part Number: AMC1350 Hi
Need clarity regarding the resistor divider network connection at the input of AMC1350. Figure below shows the current schematic for battery voltage sensing.( 0-850). But in our case there is one requirement as protection for…
Part Number: AMC1350 Other Parts Discussed in Thread: ADS1220 , , AMC3302 Greeting,
Our product implements AMC1350 and ADS1220 to measure voltages upto 200Vpk. We see a small offset that is random at startup but is consistant when the device is kept…
Part Number: AMC1350 I am using an AMC1350 for AC Mains monitoring and have found that it draws a slug of current on VDD2 at the negative zero crossing of the input waveform at INP, with INN tied to GND1.
Is this to be expected? There are 1uF decoupling…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC0386 Hi,
We are using AMC1350 for voltage sensing. Our requirement is to get 0.1 % accuracy in sensing the voltage. We have to chose resistors such that we get 0.1 % accuracy and power loss of…
Part Number: AMC1350 Other Parts Discussed in Thread: TLV9051 Given below is the schematics and simulation diagram of the battery voltage sensing circuit used in the chopper board. The marked section in the simulation diagram is the input side of the…
Part Number: AMC1350 I have a question about the input voltage of the AMC1350.
It is specified as ±5 V input, but the absolute maximum ratings (P4) list MIN: -15 V and MAX: 15 V.
If a noise spike exceeds ±5 V even for a single pulse, could that cause…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC3330 Tool/software: Hi,
is it possible to use the AMC1350 in the following configuration to measure the Neutral Point Displacement?
Part Number: AMC1350 Other Parts Discussed in Thread: ISO224 Hi Team,
Posting on behalf of our customer.
I am considering the AMC1350 isolated amplifier for use in an audio application and would like to inquire about its suitability for this purpose…
Part Number: AMC1350-Q1 ■ Target Product TI Isolated Amplifier / AMC1350-Q1
■ Inquiry Content 1. I would like to connect the secondary side (OUTP, OUTN) to a single-ended input circuit (ADC input of a general-purpose microcontroller). Do you have any…