Part Number: AMC1350 Hi,
I have a senario where the analog input voltage to AMC1350 might be present when the device is off i.e. VDD1 is off.
The datasheet specifies absolute max. analog input voltage of ±15V, without any reference to VDD1, and input…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC1351 , AMC3330 Hello TI Team,
I am currently in the process of designing an AC/DC voltage sensor utilizing the AMC1350 isolation amplifier and would greatly appreciate your expertise in verifying…
Part Number: AMC1350 Tool/software: Hi
I am doing worst case analysis using .wcca function and monte carlo simulations in LT Spice. Currently using the Spice models of AMC1350 & OPA320A for simulation.
I wanted to know whether the different types…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC3330 Tool/software: Hi ,
I am attaching the input section of battery sensing circuit.
I needed to know whether the pin connections of AMC1350 are correct or not ? Whether it will work for…
Part Number: AMC1350 Hello,
I am currently using the AMC1350 in a sensing circuit for a High voltage amplifier. the output waveform of the amplifier is 15kHz Sine @ 4000Vpeak centered at 0V, which is fed into the top of the resistive divider in the…
Part Number: AMC1350 Tool/software: MPN:AMC1350DWVR Regarding the wire bond, this is not a transition from gold wire to copper but rather an additional assembly. The PCN states that ONLY the parts assembled in MALAYSIA are having copper to copper die…
Part Number: AMC1350 Tool/software: Hi
I am currently working with the AMC1350 to provide reinforced isolation for a voltage sensing circuit. My input signal is 100 V peak-to-peak sine wave, which is stepped down by a factor of 0.0021 using a voltage…
Part Number: AMC1350 Other Parts Discussed in Thread: ISO224 Hi, I am in need of a differential input, isolated opamp. I am currently trying to use the AMC1350 for CM rejection. I have attached my schematic:
V8 is Common Mode voltage.
My question…
Part Number: AMC1350 Tool/software: Hi team
There are two questions. Could you help these?
- As the datasheet recommends a low-ESR caps as below figure, could you tell what value of ESR are recommended? I hope to get the answer that less than xx Ohm…