Part Number: AMC1350 Tool/software: Hi,
i am using the AMC1350 in a dual configuration to measure the voltage across a DC-link.
With reference to the attached schematic:
DCP-VM voltage is positive (0 / +5V)
DCN-VM voltage is negative (0 / -5V…
Part Number: AMC1350 Other Parts Discussed in Thread: ISO224 Dear team,
We have the bio-directional current sensing application, which requires the input voltage range of ISO-AMP should be large than +_1V. We found that AMC1350 is a good choice…
Part Number: AMC1350 Other Parts Discussed in Thread: AMC3330 Tool/software: Hi Team,
Please help analyze the issue of output voltage distortion when using AMC1350 to sample three-phase AC voltage.
The original input voltage and power supply voltage…
Part Number: AMC1350 Other Parts Discussed in Thread: TINA-TI Tool/software: When using a charge pump to power the high-side VDD1, it is important to know the IDD1 characteristics.
In section 6.9 the broad definition "IDD1≤8.1mA @ 3.0V<VDD1<3.6V", and…
Part Number: AMC1350-Q1 Other Parts Discussed in Thread: AMC1350 , THS4551 , ADS8411 Hi,
I am trying to drive an SAR ADC with the AMC1350 without success. The ADC ref is AD4005 (16-Bit, 2 MSPS/1 MSPS, Precision, Differential SAR ADCs). The observed…
Part Number: AMC1350 Tool/software: Hi Team,
What's the min and max value of differential voltage? Both INP/N and OUTP/N. Customer is asking it for design. I don't find it on datasheet.
BRs,
Francis
Part Number: AMC1350 Dear Team,
I am using AMC1350 in one of my application. Please see the below circuit.
You can see that the voltage at the input of AMC1350 is 2.294V
The expected voltage at the input of AMC1350 is 2.3766V
I believe the…
Part Number: AMC1350 Other Parts Discussed in Thread: INA290 Dear Support Team,
I would have a partially connacted question. Would it be somehow possible to detect short circuit using one of above meantioned chip (INA, AMC, LMP etc)?
Thank you very…
Part Number: AMC1350-Q1 Other Parts Discussed in Thread: AMC1350 , , TINA-TI Hello, I am planning to connect a RC filter on the output of AMC1350. The spec says that if R=0 the max. "OUTP to OUTN" cap is 250pF. How can I determined the maximum capacitor…