Other Parts Discussed in Thread: UCD9244 , UCD74120 , UCD9224 Hi all,
I used UCD9244+UCD74120 to generate 1.0V to supply the Keystone II SOC's core power.
Now we have not mounted the SOC yet. We just debug the UCD9244+UCD74120.
And I met a problem…
Hi Senthil
Thanks for your replying.
We have purchase a K2HX and K2H evm. According to this thread,
It said that the K2H using 66AK2H12 and K2Hx using 66AK2H14. I want to make sure that what I have on our K2Hx is 66AK2H14. From the BOM provided…
Thanks!
I refers this schematics K2H_K2EVM-HK_SCH_A104_Rev4_0.pdf
In page 40, you will see one UCD9244 that is U16 controls two UCD74120s that are U10 and U44 simultaneously.
So is this design is not good enough? Actually one TI engineer shows me…
Part Number: DS90UB934-Q1 Hi Ti Team,
They used DS9UB933-Q1. We used T123AI chip to drive the screen and do some other functions. How to pair DS9UB934 with T123AI? Or is there a more suitable chip recommended?
T123AI.pdf
Thank you, Timothy.
We think it is the loop compensation issue. We used the design in below quickstart calculator, and the issue of startup was solved. However, in the Bode Plot, you can see the loop bandwidth is very narrow, and the slope is -40db…
Part Number: AM5708 Other Parts Discussed in Thread: AM5728 Hi:
I have a custom AM5708 based board with SDK6.02 Linux RT.
The board has 3 ethernet interfaces:
- eth0: connected to GMAC
- eth1: connected to prueth pruss2_eth
- eth2: connected…
Hello Ki,
Thanks for looking into the issue.
Attaching two files.
build file --> build.txt
output file --> project_zero_CC26X2R1_LAUNCHXL_tirtos_ccs.out
Regards,
Pothirajan.K
/cfs-file/__key/communityserver-discussions-components-files…
Part Number: TMS320F28335 Tool/software: Code Composer Studio Hi everybody,
i have a board which is produced by Technosoft. The boad has a f28335, RS232, and JTAG pin. The board is connected to pc via RS232. Normally the card has a special program and…
Hi,
Attached file is the previous version 5.12 of CMRT released by TI on Oct - 2019 but we need new version 6.01 in this year. Please help providing the CMRT 6.01 version. Thanks!
Best Regards,
Susan Chen
Spectrah Dynamics, Inc.
5F-2, 188…
J721E_registers2.pdf
hello Sarabesh
The attachment is the register manual. Specific chapter: 7 ENCODER Registers.
Which registers indicate the working status of buf and encoder?
Is the VIDIOC_QUERYBUF command used to query the status of buf? …