Part Number: CDCM7005-SP Other Parts Discussed in Thread: CDCM7005 We have implemented a CDCM7005 in our equipment for clean clock generation. It synchronise to external 50 MHz reference clock and generate in particularly a clean 100 MHz. We have been…
Part Number: CDCM7005-SP we are using CDCM7005MHFG-V clock synthesizer, we required IBIS model for SI but in ti website there is a 3 different IBIS models are available so kindly suggest us which one is latest one.
Hi,
It seems Fancort has not published the updated version which I have attached here showing the correct dimensions. Also, the end of the datasheet provides more detail on dimension "C" just below the the graphic you have provided (see below).
…
Part Number: CDCM7005-SP
Can we configure output clock as combination of 2 channel (2X2) LVCMOS and 3 channel LVPECL?
If configure as LVCOM , what will be the phase difference between Y0A and Y0B, means both clock will be in phase or inverted clock…
Part Number: CDCM7005-SP Other Parts Discussed in Thread: TLK2711-SP , CDCM7005 , Hi,
i would like to use CDCM7005 to generate the clock for TLK2711-SP.
1. If i use CDCM7005-SP in the distribution mode, will it meet TLK2711-sp's requirement of 40ps…
Part Number: CDCM7005 Dear Sir/Madam,
I would like to find out the different between CDCM7005 and CDCM7005-SP.
1) Does both space and industry grade using the same process technologies node, eg same die design?
2) If both is the same process technologies…
Part Number: CDC-CDCM7005-CALC Hello,
in CDC-CDCM7005-CALC, there is a parameter, Gain peaking. For considering loop stability, I think we can check phase margin typically, like phase margin has 60dB or like that.
Does gain peaking affect to loop…
Part Number: CDCM7005-SP Other Parts Discussed in Thread: DAC5675A-SP Hello,
In my case I use CDCM7005-SP and DAC5675A-SP, I download CAM file from TI . When I opened the .bxl file with the Ultra Librarian software, It shows that:"Can not display footprint…