On my base station board the IC is a CP2102.
Please let me know if there is any other information I can give or anything else I can do to help. Thanks very much
-Eric
A while back I wrote up and posted to Github a project that dealt with embedding a generic USB-to-serial adapter (FT232RL, CP2102, CH340G) in MSP430G circuits so firmware updates could be flashed by users via BSL with only a USB cable - no other programming…
Part Number: TMS320F28379D Hi E2E team,
I am running sci_echoback example and with some minor modifications (GPIO9 and GPIO8 for RXD and TXD) I am seeing some garbage characters instead of alphabates.
The code I am running is here:
//###########################################################################…
Florian -
you have verified the HW is good with our GUI or other COM Port "packet builder" program? this will indicate which way to go...
BTW - what is the HW setup? Is this just our EVM or your design? If it is our EVM, did you load the USB driver…
Other Parts Discussed in Thread: HALCOGEN For a project i need the sci communication. I am using the LaunchpadXL2 570LC43 so the TMS570LC43x from TI. So i use Halcogen and CCS for the programming (and TeraTerm so far).
i want to send some data over…
Other Parts Discussed in Thread: LAUNCHXL2-570LC43 , TMS570LC4357 , HALCOGEN , TMP006 Hi Guys,
i have a Problem. I am kind of new to the programming world. My goal is to read the current temperature from the Temp.Sensor 1 on my TI Launchpad LAUNCHXL2…
I think its not the problem with the voltage levels. When i checked the electrical parameters of CP2102 it was like this:
Electrical parameter:
- Voltage supply for USB: DC 5V
- Current consumption: Max 30mA
- Output high level: >2.8V @ 10mA load…