Hi Carl ,
The slow rise time of the inputs signal you mentioned in your post , how slow is it ? It is not recommended to have slow transition rate input signal into the device for its inherent issues . I have attached an app note talking about it .…
Hi Tony,
Tony B44 said: can I trade off the bitrate for quality Yes you can control the bitrate & Quality.
You can generate the sample video clips at your platform using the library in .
The user guide in Docs will provide you more details on bitrate…
Could you please try the following:
1. Download the file attached. Change the extension from .txt to .bin
2. Run it from the command line with the following parameters:
"ti_simpack_vayu_ccs_0.6.2.0_setup.bin" --mode silent --prefix "/home/vasanthaangappan…
Hi Praveen,
I referred the section 3.6.5, optimized frozen graphs for MobileNet and tried to run the generated .pb but it's also showing error in tidl_log.txt file as :
"
TF Model File : ..\..\test\testvecs\config\tensorflow_models\mobilenet\mobilenet_v1_1…
Hi Mario,
You'll need to install the python module missing via pip (a python package manager) to get rid of the error (crcmod mod in this case).
Perhaps, instead of running the python script through python, use the executable (that already has all…
Hi Karl,
You're running Windows 7, what's the service pack? We require service pack 1 or higher.
Please post the logfile created (<installdir>/install_logs/MSVC_REDIST_2008.log) here.
I'd like you to run the executable on the command line in interactive…
Part Number: TDA2 Tool/software: TI-RTOS Hello, I'm running the TIDL object detection usecase, and usecase is running fine only with a small problem here:
My original input file is .MP4 with resolution 1920*1080, and I make it to .h264 with resolution…