Part Number: IWR1642BOOST Other Parts Discussed in Thread: IWR1642 Hello!
I believe I may have a hardware issue with my IWR1642 BOOST. I've used the firmware for the people counting demo (tried both versions 2.1.2 and 2.2.0) and I'm reading the frame…
Part Number: TPS65982-EVM Other Parts Discussed in Thread: TPS65982 Hello,
We are trying to use the TPS65982-EVM as a dock for a smart phone that has a type-C connector such that the phone will accept a charge, but still act as a host. This seems to…
Part Number: PROCESSOR-SDK-DRA7X Tool/software: Linux How to implement Wakeup on CAN message on TI J6 EVM.
Guidelines to implement RTC mode on TI J6.
How DCAN1_RX (AD17) configure to CAN rx and Wakeup 0 source.
Other Parts Discussed in Thread: DRA742 Hi,
I need to port the bluetooth driver for the below platfrom
CPU : DRA752-GP ES1.1 Model: TI DRA742 Board: DRA74x EVM REV G.0 DRAM: 1.5 GiB
Can you please share the correct schamtics.
Best Regards, …
Part Number: DP83867ERGZ-R-EVM Hello,
i have questions regarding the output impedance control setting of the GBit PHY DP83867.
The output impedance can be configured with Bit 4:0 in the I/O Configuration Register (IO_MUX_CFG) with address 0x0170…
Part Number: UCC28881EVM-680 Other Parts Discussed in Thread: UCC28881 Dear Sirs,
When loading 0-130ma with TI UCC28881 EVM (UCC28881EVM-680), the board makes a harsh sound.How to solve this issue? Thanks!
Hi, Ji.
While reading your questions and replies, I have a question about your attempt to use Direct mod 0.
When I saw the datasheet about trf7960A evaluation module, I guess I cannot use Direct mod 0.
However, you tried. So i wonder you acheived…
Part Number: AWR1443BOOST
Hi.
HW: AWR1443BOOST + DCA1000
SW: Radar Studio
Place the AWR1443BOOST in a chamber and the metal object is 4 meters away from EVM.
We start to rotate AWR1443BOOST along the Y-axis from 0 degree to 20 degree like…
Part Number: TDA2 Hi master:
My board is TDA2EVM [VAYU EVM XC5777X CPU BOARD]
The board run OV10635 camera well, the des out raw is [2~9],
now we need to use another camera the des out raw is [0~7],
How can I set the board?
thanks.
kevin…