Part Number: TRF7960A Hello,
I try to use Direct mode 0 function in trf7960a.
Trf7960a transmits only 13.56MHz carrier signal. Depending on the load which is controlled by data value from a circuit, I want that carrier signal has different amplitude…
I have two C6657 EVMs connected with a HyperLink cable. The slave EVM is booting up in the HyperLink ROM bootloader mode. I've verified by reading the remote registers on the master EVM that all of the address mappings are the defaults used by the ROM…
Part Number: TRF7970A We have bought a TRF7970A EVM for measuring the ISO15693 tag responds to the request and the subcarrier data .
According to the TRF7970A datasheet(SLOS743L page46), we use GUI to set the register as follows to enter direct…
Other Parts Discussed in Thread: TPS65986EVM Our customer tried the following configuration and DP ans USB functions worked fine.
Notebook--USB/DP Source--> DP EXPANSION(source) + TPS65986EVM <--type-C--> TPS65986 EVM + DP EXPANSION (sink) --Monitor…
Part Number: EVMK2EX I am booting the Keystone 2 66AK2Ex board via tftp and ramfs using these pre-built components from SDK ti-processor-sdk-linux-rt-k2e-evm-03.03.00.04.
board-support/pre-built-images/zImage-k2e-evm.bin board-support/pre-built-images…
Other Parts Discussed in Thread: OMAP-L137 Hi,
I'm using Spectrum Digital EVM for OMAP-L137. The PSP version is DaVinci-PSP-SDK-03.20.00.14
I'm trying to boot Linux kernel from SPI flash by following the wiki page:
http://processors.wiki.ti.com…
Hi,
we are slowly making progress in getting our Mistral EvalBoard working with SYS/BIOS for ARM and DSP (thanks to Pavel).
However, now we are facing the next issue: The board is shipped with a 256MB Micron NAND Flash (MT29F2G16ABAEA) which has a…
Hello,
My customer is trying to boot the device from SPI NOR, Ethernet, etc on C6678 EVM and they got stuck if big-endian was being selected. Please note they have verified the boot was succeeded with little-endian mode. From my investigation, I noticed…
Part Number: 66AK2E05
Tool/software: Linux
Hi,
As a follow-up of the question I posted here:
https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/610616/2253544#2253544
I tried booting up using "env default -f -a" and in "name_fs", I…
Part Number: AM5728 Tool/software: Linux Hi,
I am testing AM572x boot up with Linux OS( using SD card) on AM572x EVM.
I have boot fail once each 100 times. At that time, I see the error message.
[ 18.454801] alg: skcipher: Chunk test 2 failed on…