HI Anshu Madwesh,
The following is the log of waking up via USB when the TMDS62LEVM board enters RTC+DDR mode.
root@am62lxx-evm:~# echo disabled > /sys/devices/platform/bus@f0000/f900000.dwc3-usb/power/wakeup
root@am62lxx-evm:~# echo disabled > …
Hello Hao Teng,
hao teng said: Since it is a self-made board, may it be related to the slow power supply time of dp83867? I am planning to test the power supply time of dp83867 and am62 simultaneously. Do you have any direction for troubleshooting?…
Part Number: DP83867E Tool/software: Hi Team,
I was looking for TSN compliant Ethernet controllers and found DP83867 part. While referring to the EVM DP83867E Dual-Port TSN PCIe Application Interface Card schematics, PCIe host interface page, the PCIe…
Part Number: DP83867E Tool/software: I am interested in implementing PTP in my application and I've read over the document, "How to Configure DP83867 SFDs" ( How to Configure DP83867 Start of Frame Detect ), but it was not clear when or where the necessary…
Part Number: AM6548 Other Parts Discussed in Thread: DP83869 Tool/software: Hi,
I am using the AM6548 with a new PHY transceiver. The IDK evaluation design uses the DP83867 PHY, but I am using a design with a DP83869. When I run the MDIO list command…
Hi Ajit
You can use Wurth Elektronik 7499111000A RJ45 Magjack Connector. This component has been used on the DP83867 EVM in the past so we have a history of validating our parts with it.
Thanks
David
JH
I am looking at their RJ45 connector and it is not an RJ45 connector as shown below.
Before we look at the RGMII side, are they able to link up with DP83867 link partner?
Thanks
David
Hello Nick,
Thank you for your support. I raised this ticket a while ago there have been updates, but I was unable to add them to the ticket. Currently ethernet is working but only when using CPSW. ICSSG has not yet been resolved, however I need to…
Hi Liam, The only write was 5448. Bit 10 forces 1G link on DP83869.
Liam Borg said: In 1000Base-T to 1000Base-X mode in the above setup the LED 0 and 1 blink on power on the turn off after a few seconds. If i disable link loss LED0 doesnt change, but…
Hi Conor,
I am unsure about your first request. If the EVM passes compliance test, then it can be said that the PHY can as well. Conversely, in a theoretical sense, you can use that same PHY DUT and have very poor design and layout techniques and have…