Part Number: DS90UB902Q-Q1 Other Parts Discussed in Thread: DS90UB901Q-Q1 , Hi,
My dashboard's interface is BT656:8/10/12bit, so I select DS90UB902Q-Q1 as deserializer. From the datasheet, the recommended serializer is DS90UB901Q-Q1. But in my application…
Part Number: DS90UB902Q-Q1 Hello, We use in combination of DS90UB901Q and DS90UB902Q. There is a issue that the LOCK signal of DS90UB902Q falls to low occasionally and CRC errors occur(Pass signal to high). We using Both DS90UB901Q and DS90UB902Q in Slave…
Part Number: DS90UB902Q-Q1 Tool/software: Code Composer Studio Hi
I design a circuit of DS90UB902 chip to decode the LVDS signal from the camera!
I select the camera mode which set the remote DS901 M/s = L; PDB = H; Res = L,
The DS90UB902 configure…
Part Number: DS90UB902Q-Q1 Tool/software: Code Composer Studio Hi
I design a circuit for data transmission by DS901 and DS902 between the ECU and camera.
I used the GPIO[0:1] as UART for the communication.
as follow
And configure the 902…
Part Number: DS90UB902Q-Q1 Other Parts Discussed in Thread: DS92LX1621
We are attempting to use a DS90UB902Q deserializer in some test hardware receiving data from the DS92LX1621 part. It is an imaging/camera application with the DS90UB902Q receiving…
Part Number: DS90UB901Q-Q1 Other Parts Discussed in Thread: DS90UB902Q-Q1 , DS90UB926Q-Q1 Hi team,
As we know, we always uses DS90UB901Q-Q1 with DS90UB902Q-Q1. The customer would like to get if he can use DS90UB901Q-Q1 as the serializer, and use DS90UB914Q…
Hi Ersin,
I have copied the information from the link below:
1) The information we can provide on the DS92LX1622 Reg. 0x27 is limited, as this register involves specific factory design parameters. In summary, Reg 0x27[7:0] are BCC parameters that…
Part Number: DS90UB926Q-Q1 Other Parts Discussed in Thread: DS90UA102-Q1 , , DS90UB904Q-Q1 , DS90UB902Q-Q1 , DS90UB914Q-Q1 , DS90UB914A-Q1 OUR CASE WILL USE FPD-LINK PARALLEL DESERIALIZER BUT HERE ARE POOR OF PARALLEL INTERFACE.
PLEASE SEE BELOW DIAGRAM…
Part Number: DS90UA101-Q1 Hello High Speed Interface Forum, please see question below:
The DS90UA901/902 SERDES combo with the DS90UB913/914, I see that the 913/914 pair costs less and it appears to be in higher supply:
DS90UA101-Q1
…
Other Parts Discussed in Thread: DS90UB901Q-Q1 , DS90UB902Q-Q1 Dear sir,
We try to connect NS LVDS chips "DS90UB901Q-Q1/DS90UB902Q-Q1" to DM814x.
We found LVDS chip needs I2C "clock stretching" mode support on DM814x's I2C controller.
Could…