Kamalesh c said: OTA is used to upgrade some features through the air ?
Yes, OTA means over the air firmware update.
Kamalesh c said: upgraded features can occur in which place of the process ?
where the upgraded one ?
Please refer to section…
I went back utilising the ready made Port2 interrupt handler in io_pins.c and there is the __low_power_mode_off_on_exit() which should clear the SR register bits, thus disabling the low power mode in ISR exit, as far as I understand. (It's a bit misleading…
Part Number: MSP430FR2476 Other Parts Discussed in Thread: MSP430FR5994 , MSP430FR2433 We need to create a boot for the MSP430FR2476 microcontroller.
We are basing ourselves on the document slaa721e "MSP430FRBoot – Main Memory Bootloader and Over-the…
David,
I was able to reproduce this bug with the following common setup:
-IAR 7.60.1.11216
-MSP432401R development board
-TI Flash example code, below.
Any other ideas on a fix? The IAR update did not seem to do anything.
Thanks for the…
Part Number: TM4C123FH6PM Tool/software: Our application can update itself and then needs to restart.
The SysCtlReset() call only works when it is executed from privileged mode (f.i. in an interrupt). In order to be able to use it, I would like to trigger…
Of course, thanks for making the update.
Can you verify that you are using the MSPM0G3507 Launchpad, as opposed to another MSPM0G device such as the MSPM0G3506? Additionally, could you specify which version of code composer studio you are using?
The…
Part Number: MSP430G2231 I have an old MSP430 design that started with earlier CCS versions 4 or 5. The devices was in-use and has worked for years, and suddenly stopped responding.
It is using theMSP430G2231 as shipped on the Launchpad board with USB…
Hi,
If it helps, SDK 5.10 has been tested with IAR Embedded Workbench: EWARM-8.50.9.
You will get more insight on the compatibility between IAR Embedded Workbench versions by contacting IAR Systems. You may also want to review the release notes of…
Please see my answers below:
What model/version MSP430-FET?
- It's MSP-FET Flash Emulation Tool ( https://www.ti.com/tool/MSP-FET
Windows, Linux or MAC?
- Windows 10
What version of IAR are you using.
- 7.11.2
You indicate that it…