Other Parts Discussed in Thread: INA217 Hi,
I make one tda2052 amp.60W only, How I interface it with the Digital volume
Controller with an IR sensor circuit add as a remote controller.
OR
it with INA217
Andrew,
we have other low noise instrumentation amplifiers like the INA163 and INA217, but they are not available in the MSOP-8 either. The INA163 comes in a narrow body SO-14 package.
Best regards
Frank
Other Parts Discussed in Thread: INA128 , INA217 , INA163 , PGA202 , PGA206 Working with INA128, single supply, ac coupled, driving high pass, single-pole RC filter with impedancee around 17 kohms. I see that the gain vs frequency has shifted away from the…
Other Parts Discussed in Thread: INA103 , INA101 , INA111 , INA114 , INA115 , INA116 , INA118 , INA121 , INA128 , INA129 , INA163 , INA217
Hi
I use an INA103 in the same configuration as shown in figure 1 (page 9) in the datasheet. The differential voltage on…
Other Parts Discussed in Thread: OPA1612 The input of the circuit has a balanced input but, the output is unbalanced. I would like to know what circuit i have to add for get a balanced output
thanks