Part Number: INA228 Other Parts Discussed in Thread: INA4230 , INA4235 Hi,
We design a circuit with the following specifications:
Ultra low power consumption (in standby, when measurements are off)
Measure 3 voltage rails:
4-15 V
4-15 V …
Part Number: INA228 Hi sir,
The VS pin need external power to offer, could we use 12V that we want to monitor one divide to right value for it?
The screenshot is capture from your spec., the monitor accuracy is 0.5% for full scale, was it include…
Part Number: INA228 Hi,
The I2C interface on my desing is on a 1.8V bank IO of FPGA and I am trying to connect the INA228 directly without votlage level translator, based on the INA228 datasheet that minimal VIH for INA228 is 1.2V, can I pull the i2c…
Part Number: INA228INA228_test_SCH.pdf
I need to measure currents between 50uA and 5A using the attached circuit diagram.
Is there any other way besides changing the resistor value? (If I need to reconfigure the circuit, please recommend any reference…
Part Number: INA228 Can the INA228 measure bidirectional current via i2c, and can the ALERT pin trigger on both positive and negative overcurrent events across the shunt. (bidirectional overcurrent trigger)
Part Number: INA228 Hi
I need to read the standby current and would like to know what the minimum current that the INA228 can read is given its design. Thanks
Output current 2A max
Output current 11A max
Part Number: INA228 We want to monitor the energy of a supercapacitor storage system using the INA228 via I2C.
Our currents are very high (around 100A continuous, with short peaks up to 200A), so we would like to avoid using a traditional shunt resistor…
Part Number: INA228-Q1 Other Parts Discussed in Thread: INA228
Tool/software:
I am facing issues in reading some parameters in INA228. Current, power, energy and charge registers are zero. I am able to read the shunt voltage and the voltage being…
Part Number: INA226 Other Parts Discussed in Thread: INA228 Dear TI team, I am using INA226/ INA228 in my design but when i checked the digikey and mouser to source the component, its showing out of stock. Could you please help me how i can purchase the…
Part Number: INA228-Q1 Hi
We are using INA228AQDGSRQ1 in our retarder ECU design for measuring current on the o/p of the coil MOSFET. WE have 4 coil MOSFETs.max current is 50A. we have used 4 of these devices and connected to our microcontroller FS32K144HAT0MLHT…