Part Number: INA350 Other Parts Discussed in Thread: INA351 , TLV9041 Tool/software: Hello TI Team,
We intend to use INA350 to interface the thermocouple. So could you please suggest the design ?
----------
Regards
Keyur Parikh
Part Number: INA350 Tool/software: The title of the INA350 datasheet states that the power supply voltage is 1.8V to 5.5V, but page 8 states that it is 1.7V to 5.5V. From what voltage to what voltage can operation be guaranteed?
Part Number: INA350 Tool/software: Hello,
Suggested design does not wirk as a required with INA350. Could you please check and let me know further solution.
Part Number: INA350 Hi everyone,
I have a problem with INA350CDS. I'm trying to read the temperature from a PT1000, connected to a Wheatstone bridge. I powerised the instrumental amplifier at 3V3, but the output resultan gets saturated around 0,6V no…
Part Number: INA350 Other Parts Discussed in Thread: LM358
Tool/software:
Hi! I'm having some major gain issues with the INA350AB. The circuit is an (supposed to be precision) ohmmeter for 1~30 ohms.
U11 is a LM358 or equivalent. The circuit is…
Part Number: INA350 Other Parts Discussed in Thread: RCV420 Hi ,
I am trying to measure
min current - 4mA
max current - 20mA
four wire 4-20 current loop
Vcm-12V
Vs=3.3V.
The part I would like to use is INA350 Just would like to know if it…
Part Number: INA350 Other Parts Discussed in Thread: INA351 Tool/software:
When REF connect to GND, this circuit output 8.86mV.
When REF connect to 1.65V, this circuit output 1.65V.
Why does different REF get different offset?
When REF=1…
Part Number: INA350 Other Parts Discussed in Thread: TL331B Tool/software: Hello, I'm using the INA350 with a bipolar +/- 2.75V supply but trying to control the GS pin using a 3.3V GPIO. It seems that to achieve logic-low I need to drive GS below -2.55V…
Part Number: INA350 Other Parts Discussed in Thread: TINA-TI , INA351 Tool/software: Please find attached a small TINA-TI simulation of INA350. When the two input resistors are each 200kOhm, the gain gets killed down to 0dB. When I change to 0ohm, the…
Part Number: INA350 Other Parts Discussed in Thread: TL431 , TLV9061 Tool/software: I have a sensor with an output range of 50mV to 500mV relative to ground. I need to convert this signal to a 0-5V range (or another suitable range) for measurement with…