Part Number: ISO124 Tool/software: Is it possible to isolate a differential signal using two ISO124s?
please check attached file.
ic133 and ic135 are iso124.
input signal range (in0+ to in0-) is between ±5v and 0v.
if thera is a problem,tell me…
Part Number: ISO124 Other Parts Discussed in Thread: ISO224 Tool/software: CAN I USE ±10V INPUT SIGNAL UNDER the CONDITION?
+VS1 :5V
-VS1 :-5V
+VS2 :+5V
-VS2 :-5V
±VS1 AND ±VS2 are isolated.
Part Number: ISO124 Other Parts Discussed in Thread: TL071 Tool/software: Hello,
The customer uses ISO124 for signal isolation, as shown in the circuit diagram below. The signal is used to drive the frequency converter, with an input voltage of 0-10V…
Part Number: ISO124 Tool/software: The ISO124 data sheet states that the "Initial offset" is +/-20mV typical.
What do they mean by "Initial" and how much time after the "Initial" period can the part be expected to drift?
I also need to know the magnitude…
Part Number: ISO124 Other Parts Discussed in Thread: OPA2990 , ISO224 , Hi Team,
I need you support for new design. requirement is taking potentio meter output to rc filter--->buffer opa2990 >> divider(1/8)---> ISO124U ---> ADC PIN OF MCU.
Supply…
Part Number: ISO124 Tool/software: I want to use this IC for NTC thermistor temperature sensing for IGBT module . Can I give +15V to -10V for Bus side supply to this IC . Other side can I give only +5V to GND will the IC works?
Part Number: ISO124 Other Parts Discussed in Thread: AMC1411 , ISO224 , AMC1400 Hello:
Can I connect VS1- to GND1? I want to use a single power supply.
Below is my circuit diagram
Part Number: ISO124 Tool/software: According to the manual, ISO124P has two functional modules, G=6 and G=1, inside. In reality, the external output of ISO124P is 1. If the internal G=1 module or 200kΩ or A2 fails, will it cause the output ratio to increase…
Part Number: ISO124 Other Parts Discussed in Thread: ISO224 Hi,
I am going to design a circuit to isolate the ground between 2 sides. So, i planned to go with ISO124. I have some queries related to it.
Input Voltage range : 0V to 10V
Power supply…
Part Number: ISO124 Other Parts Discussed in Thread: ISO224 , AMC3330 , AMC1350 Hello,
I am working on the high voltage sensing circuit design. I would like to use iso124 or iso224 to be a isolator. input voltage can be phase to neutral (120V, 250V…