Part Number: TDA4VM
Hi TI
There's a question that customer wants to get clarified about compatibility of LPDDR4 device.
They consider to use H54G46BYYPX053 rather than MT53D1024M32D4DT due to delivery and cost issue.
I tried to check the specification…
Part Number: 66AK2L06 Other Parts Discussed in Thread: TCI6630K2L Hi all,
I have worked on booting up secondary ARM core(aka CPU1) on 66AK2L06 almost two weeks with failure all the time.
I am using ti-processor-sdk-linux-k2l-evm-03.03.00.04(and also…
Hi Nick,
here are my DTS and the boot log. I'm having the problem with PRU0 of ICSSG0 and ICSSG1.
// SPDX-License-Identifier: GPL-2.0
/*
* Copyright (C) 2016-2018 Texas Instruments Incorporated - http://www.ti.com/
*/
/dts-v1/;
#include "k3-am654…
Other Parts Discussed in Thread: BQ24171 Hi all,
I am using a custom board which has a imx6 processor running on Android kitkat 4.4.2. The bluetooth works fine at boot up but when disable the chip (pull down the BT_EN pin to low) at suspend state…
Yea, I used the default config. I also used a multimeter on the usb port and even if I turn off then back on no voltage is supplied to the USB port. Here you go:
/proc/config.gz
#
# Automatically generated file; DO NOT EDIT.
# Linux/arm 3.12.10 Kernel…
Other Parts Discussed in Thread: TMS320F28335 , CONTROLSUITE Dear all,
I have problem to make external mode with eZdsp TMS320F28335.
I use matlab 2016, I install ControlSuite+CSSV6 in the same directory TI.
I download the package C2000 from mathwork…
Hi Rachel,
I have changed the following preprocessor settings in the Host Test project:
MAX_NUM_BLE_CONNS=4
MAX_PDU_SIZE=207
MAX_NUM_PDU=4
I suppose they can't influence Host Test application in such manner.
Also I have reproduced this issue…