Part Number: LM2903B Other Parts Discussed in Thread: LM2903
Hi,
I am using LM2903 Comparator with hysteresis in my circuit. Circuit is as shown below image. I want to know the formula to calculate the Hysteresis (Both High Threshold & Low Threshold…
Part Number: LM2903B-Q1 Other Parts Discussed in Thread: LM2903B Hi Expert,
I'm calculateing the value of the hysteresis input with LM2903B.
However I found the difference between similation results and caliculation results.
Could you please let…
Part Number: LM2903B-Q1
At this time, I would like to analyze the performance of the LM2903B-Q1.
I did some manual calculations and simulations (with SIMetrix) to make sure the simulation result.
To make the context, I try to simulate the comparator…
Part Number: LM2903B Other Parts Discussed in Thread: TL331 Ich nutze den Komparator TL331I für die Simulation in PSpice.
Für den Grenzentest beträgt die Versorgungsspannung 2.6V.
Die Spannung am - Pin(türkis) beträgt ca. 850mV.
Die Referenz am…
Part Number: LM2903B-Q1 Other Parts Discussed in Thread: LM2903B , LM2903 , LM339 Hi - customer question below:
If 13.5V is applied through 49.9kOhms to the (+) input of a LM2903B that has no power applied to it (VCC=0V), is there any kind of positive…
Part Number: LM2903B-Q1 Other Parts Discussed in Thread: LM2904B-Q1 Hello,
do the datasheet parameter input offset voltage and input bias current in the datasheet of LM2903B-Q1 and LM2904B-Q1 include aging?
Thanks and best regards,
Michael
Part Number: LM2903B-Q1 Other Parts Discussed in Thread: LM2903-Q1 , LM2903B Hi,
Could you please let me know the Quiescent current of LM2903-Q1? The LM2903-Q has 2-ch comparators and datasheet show as below.
Is the value for 2ch? I'm much confused…
Part Number: LM2903B Other Parts Discussed in Thread: LM2903 , LM2904 Hi team
LM2903B has lower Ibias than LM2904. Does it mean input impedance is higher than LM2903?
Customer concerns that high input impedance results in weaker against input noise…
Part Number: LM2903B-Q1 Hello,team
If the input of one of the two elements is open, Will it have any effect on the output of the other element?
Regards, Saito
Part Number: LM2903B-Q1 Hi expert,
Hope you are doing well.
For LM2903B-Q1, when VCC is 0, IN+ is in 0-20mV, IN- is 0, the output is in open-drain form, why output would be pulled down? (detected as low)
Thanks.