Part Number: LM293A Hi,
Can you please confirm whether the max supply current spec in the datasheet of 1mA is for the two channel or per channel?
-Kelvin
Part Number: LM293A Hi all:
Have a reply:"The first stage, U5A, is at the biggest risk. Both the input and reference voltage exceed the limit and has the possibility of an incorrect output."
However, IN my actual test, the voltage of U5A IN+ to…
Part Number: LM293A Other Parts Discussed in Thread: LM293 , TLV3401 , LMC6772 Dear all:
The schematic diagram is as follows:
Question 1:Our products are all powered by a single power source (i.e., 5V, GND).Should the parameter "common mode input…
Part Number: LM293A Other Parts Discussed in Thread: LM293 Dear all:
For the LM293 , the input voltage should be less than 3.5V at room temperature, and 3V over temperature. We recommend the 3V limit.——This is the specification.
The "common mode input…
Part Number: LM293 Other Parts Discussed in Thread: , TLV1702 Dear Specialists,
My customer is evaluating LM293A and has a question.
I would be grateful if you could advise.
---
When the output terminal (pin 7) goes from HIGH to LOW, a drop also…
Hello Nibin,
"Cost" will depend on the temp range and offset. The more "features" you want, the more cost. Offset and temp range are "features".
The LMx93/LM2903/LM2901 family is already the lowest cost family.
The LM2901AVQPWR is the lowest…
Hi Stanley,
Please reference pages 8 and 9 on the tech note that I have attached for more information on ESD diode clamping. Additionally, you will not need to worry about phase inversion.
Regards,
Joe
snoaa35.pdf
Hi Charles,
I assume the spec you're more interested in is Input Bias Current and how your resistor divider on the front end could impact the accuracy of the comparator. Input Resistance is generally an older term used for our older parts.
It's important…