Part Number: LM3673 Other Parts Discussed in Thread: TPS65581 Tool/software: WEBENCH® Design Tools Dear friends,
I'm trying to design power management for my embedded system. There are two supply voltages in my design which is 3.3V and 1.8V. 3.3V is…
Thanks for reporting the simulation issue with LM3673. I am able to reproduce this issue and will look at fixing this issue. We will keep you updated on the status of the fix.
Regards,
Amod
I do not generally support applications with output current that low. You could use a 2 or 3 A rated device but that is overkill.
For the -3.5 V output Webench suggests LM27761 or LMZ34002.
For the 1.8 V output, Webench returned a large number of possible…
Hi,
I've attached the 2013 User's Guide for power products. Starting on page 53 you will find a selection of PWM controllers. many of these teh frequency can be varied according to external criteria.
As an example if you use a UC3842 it is a simple…
Gary,
Most any of our power controllers with dual output capability will provide the control. See attached document starting at page 50 with the dual output controllers on page 53 and 54 and choose what features you want.
Regards,
John