Part Number: LM3880 I am trying to drive an LM3880MF-1AA with an MC33161DMR2G voltage monitor. The MC33161DMR2G output is an open collector driver pulled up to 3.3V via a 10K resistor. When the the two parts are connected, the output will not release…
Part Number: LM3880 Hi team,
We find the dimension is different in the datasheet whether it’s the old or new version. Could we modify it?
Old version:
12.LM3880MF-1AB NOPB.pdf
New version (ti.com):
www.ti.com/.../lm3880.pdf
Other Parts Discussed in Thread: LM3880 Hi,
Can you please specify me the current which can be supported by the VCC pin of the sequencer LM3880 because this information is not quoted in its datasheet.
Thanks
Other Parts Discussed in Thread: LM3880 Hi,
I want to insert a voltage divider at the EN validation input of the LM3880 sequencer. To do this, I need the maximum value of the resistances of the divider? This was not mentioned in its datasheet…
Hello
If they want to reduce the current, the pull-up source could be different with the source of LM3880.
The leakage of the FLAG is up to 20nA. you have to count the leakage where the flag output is connected.
This would give your the voltage…
Part Number: LM3880 I am planning to use LM3880MFE-1AA/NOPB. Referring to datasheet, fig-10, Flag Vol Vs Vcc, my understanding is Flag Vol is controlled to less than 0.1 volts when VCC is 0.9V and above. My product will be operated between -40C to +85C…
Part Number: LM3880 i need to use the component LM3880 in a simulation, i need a software where i could find its package , because i didn't find it in TINA