Part Number: LM7322 Other Parts Discussed in Thread: LM7321 Hi.
We have noticed a voltage (2.6V) on the IN+ when we apply 5V on the IN- and we got confused by this. is this expected behaviour and is it safe to run it like this?
BR // Per
Part Number: LM7322 Other Parts Discussed in Thread: OPA1622 , TLV376 Hi
I am using LM7322QMA/NOPB which is a dual op amp. I have connected both op amps in non inverting configuration and i have used 402 ohm resistors to set a gain of 2.
if i apply…
Part Number: LM7322 **** SO# 446657 ****
Hello,
our customer mentioned tat they have 8pcs failed of 2500 purchased during the ICT test. Between pin 1 and pin 4, a resistance of approx. 30 - 200kΩ is measured.
The "good" components show a resistance…
Thanks Paul,
The supply voltages used are typically 5V single rail, also in some applications +/-5V and +/-15V.
The load will be in the range 2k to 10k resistive and up to 2n capacitive.
You have given me some confidence to keep the LM7322 in the…
Other Parts Discussed in Thread: LM7322-Q1 Hello,
My customer is very interested in LM7322-Q1 datasheet specification.
Customer’s first question is process(Bipolar or CMOS).
I asked local TI office and answer is Bipolar.
Please answer following…
Part Number: TL082 Other Parts Discussed in Thread: TLV9101 , LM7322 , TLV2197-Q1 , OPA2197 , OPA2192 Tool/software: Dear sir
Its about using tl082 on differential amplifier with single Vcc(15V and 0v) ,when input is closed to 0V the output is not…
Part Number: LM7321 Other Parts Discussed in Thread: LM7322 , OPA4991 , OPA2991 , OPA991 Is the operation identical of a single vs dual chip (LM7321 vs LM7322 for example), or does having the second opamp/comparator in the IC affect the parameters?
…
Part Number: LM73 Hello,
here is my amplifier application. There should be always neagtive voltage on the output, but there isn't...
The problem I have is with negative supply. Ultimately it's supplied with LDO which gives -5V, but until it stabilizes…
Other Parts Discussed in Thread: INA250 , LM7322 Hi expert,
Customer would like to design a 20 loops current measurement.
The test current pattern as below:
1. amplitude: 25A ( On time : 200us / Off time :800us)
2. rise/fall time: 500ns/500ns…
Other Parts Discussed in Thread: LM7322 , LM4991 Sorry if I am so late, I had to finish other tasks before getting back to this simulation. I have tried the suggested model (new, empty file, just your model a power and signal source), but something is…