Hi Marceli,
the output current of XTR111 must be limited to less than 50mA or you risk that the XTR111 becomes damaged. The XTR111 is not designed to output a current of 100mA.
I would think about using the improved Howland current pump:
3835.snoa474a…
Part Number: OPA547 Other Parts Discussed in Thread: TINA-TI Team,
We are using the OPA547 for an "improved Howland current pump" to turn voltage to a 0–20 mA output.
It works ok until a given input voltage level. When this input voltage is reached…
Hi Faisal,
A complete discussion of the Improved Howland Current Pump is covered in TI Application Report, SNOA474 (AN-1515), A Comprehensive Study of the Howland Current Pump. That should answer most any question you may have about the fundamentals…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…