Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B
Tool/software:
Hello,
I have LMK05318BEVM und it works very well.
I have been able to synchronise a 100 MHz output frequency to 1 KHz input frequency (phase and frequency) with…
Part Number: LMK05318BEVM
Tool/software:
Hello,
I have LMK05318BEVM und it works very well.
How can I determine how much time it takes the generated output frequency to get locked (phase and frequency) to the input frequency? For example, 1 KHz…
Part Number: TICSPRO-SW Other Parts Discussed in Thread: LMK05318B , LMK05318BEVM , USB2ANY Tool/software: Hello,
I am encountering the following error when clicking "Program EEPROM" in the latest TICS Pro version 1.7.8.0. Config was created in this…
Part Number: LMK05318BEVM Hi, we are attempting to use the LMK05318BEVM to discipline form a 1pps source. We have use the internal XO and an external signal generator (@12.8MHz) to no avail. With a 1pps signal on PRIREF - we are not seeing the PRIREF_VALSTAT…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B Hi ,
This is regarding the requirement of configuring the LMK05318B chip for varying reference clock when connected to a Host controller on the final finished product. Since the change…
Part Number: LMK05318BEVM Tool/software: Hello team,
Would it be possible to share the size of this EVM? (Length, Width, Height)
OR is it possible to share the 3D CAD data?
Best Regards, Kei Kuwahara
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B I also have a new LMK05318BEVM. Jumpers are set up as per the manual and the IIC is able to find the part but there is no output. The supply current is 220mA and all outputs are dead…
Part Number: LMK05318BEVM HI I was having problems with an older TI eval board so I purchased a new LMK05318BEVM. Jumpers are set up as per the manual and the IIC is able to find the part but there is no output. The supply current is 220mA and when I…
Part Number: LMK5B12204 Hi,
How can the in chip EEPROM be programmed using an external Host controller. Since as of now the TICSPRO Config file is finalised for a specific frequency plan. Hence, the proper sequence of the steps to do the one time EEPROM…
Part Number: LMK05318BEVM Other Parts Discussed in Thread: LMK05318B , LMK5B33216 I have a 10 MHz clock signal and I am attempting to create a frequency-syntonized output with a known phase offset.
I have the 10 MHz input connected to PRIREF with the…