Part Number: LMK61E2EVM Other Parts Discussed in Thread: LMK61E0M , LMK61E2
Hello,
One customer gave me the feedback that when he used LMK61xx Oscillator Programming Tool, if he click "EZ configuration "to generate configuration automatically, he…
Part Number: LMK61E2-312M50SIAR Now I want to use the chip to design the circuit of LVPECL output AC configuration,
The application circuit diagram of the following figure is recorded in the data sheet。
Question 1:How is the resistance of 150 Ohms…
Part Number: LMK61E2 Hi Team,
Our customer pointed out that they found a mistake in the device address mentioned in table 1. The table states 10110 with either 0x0, 0x1 or 0x3 . In the pin functions table, the influence of the pin address mentions 00…
Hello,
So I'm not sure I understand what is happening here...
We have tried this on the bench. Used the LMK61E2 device and the TICspro GUI and produced the correct output. Just typing in 196.608 in the output configuration frequency box and clicking…
Part Number: LMK61E2 Hello,
I am using LMK61E2 oscillator as clock source for my transceiver module. I am getting default 156.25MHz form the oscillator.
But I need 122.88MHz for my application. I am having I2C access to the oscillator. So please…
Part Number: LMK61E2 We are planning to use this part in many designs to replace another programable synthesizer that has gone obsolete. We need to give our customers the option to program in any frequency using our software utilities. Could TI share…
Part Number: LMK61E2 Other Parts Discussed in Thread: CDCE6214-Q1 , LMK04832 , LMK04808 , CDCI6214 Hello,
I am considering using two LMK61E2 devices, but I was unable to find anything in regard to synchronizing multiple devices. Since there is no reference…
Part Number: TX7516EVM Other Parts Discussed in Thread: TX7516
hi
using the EVM for TX7516 the reference Clock is fixed in the factory default 156.25Mhz. On the EVM software we do have a LMK61E2-SIAR dropdown control, but it is not seen to generate…
Part Number: LMK61E2 Hello Team,
can you confirm that the OE pin be left open to enable the part because of the internal pull-up resistor, please?
Thanks and Best Regards,
Hans
Part Number: LMK61E2 Hi expert,
I would like to know the performance different between setting the NUM/DEN as 17/1536 and 17000/1536000. Does 17000/1536000 push the fractional spur energy to higher frequencies for better filtering?
Thanks.