Part Number: LMP2022 I am using the LMP2022 in a buffer configuration for triangle wave signals that have an offset. The amps in the design are powered with a single sided 5V supply. The signals are above the closed loop bandwidth recommendation of 20kHz…
Part Number: LMP2022 Would TI be able to provide the pin damage current for the inverting and non-inverting op-amp terminals?
I assume there are steering diodes in the part that protect against over-voltage transients. I am in an application where…
Part Number: LMP2022 We have a situation where the supply voltage, normally +5V nominal, is off (assume 0V) and the V- pin is connected to ground. There is a series resistance of 14Kohms connected to pin 6 (minus input). There is an input connected to…
Part Number: LMP2022 Other Parts Discussed in Thread: LMP2021 Hi Team,
My Customer wanted to know the voltage noise density / output ripple between 100kHz and 5MHz of LMP2022?(assume unity gain, input resistance 1M Ohm, power supply +/- 2.5V),do we…
Hello Joong-hyeok,
Please see below for the lifecycle information on the LMP2022 you requested. This device is currently in production with no expected EOL.
1. Start of Production(Release date/Start of selling Point) : 2008-11
2. Discontinued or…
Other Parts Discussed in Thread: LMP2022 For any linear amplifier with 2 inputs V 1 and V 2 : output V 0 =A 1 V 1 -A 2 V 2 +Constant.
For an opamp A 1 >0 A 2 >0 A 1 approximately = A 2 but A 1 can be < A 2 or A 1 >A 2
If we define : V cm =(V 1 +V…
Other Parts Discussed in Thread: LMP2022 , OPA2277 , LMP2021 Hello everyone,
I'm going to design the adaptation part of the ADC peripherical of F28M36. I want to use a two steps, one for high impedance input and the other step with a second order amplifier…
Other Parts Discussed in Thread: LMP2022 I am building high accuracy current sense circuit using LMP2022 Opamp but i am having trouble getting an accurate simulation of common mode rejection circuit using TINA.
-Do i have to build a special circuit…
Part Number: LMP2012QML-SP Other Parts Discussed in Thread: LMP2012 , LMP2022 Hello, we've been looking into the output ripple on our parts which use the LMP2012 op-amp. The output ripple is measured to be about 18kHz, is there any theory on why this…
Part Number: ADS131M08 Other Parts Discussed in Thread: LMP2022 , Hi.
I've designed a PCB using ADS 131m08 and LMP2022 amplifiers to read 4 load cell outputs.
I've tested it and there is no problem.
But, I want to remove the external amplifier and…