Part Number: LMX2594 Other Parts Discussed in Thread: ADC12DJ3200 , LMX2582 , , LMK04828 , TIDA-01410 Dear Sir,
Already we are using the 2 nos of ADC12DJ3200 device by providing common clock from LMX2582 and validated the phase synchroinzation between…
Part Number: ADC32RF45 Other Parts Discussed in Thread: LMX2582 , LMK04828 , LMK04610 Doing an architecture analysis for a proposed receiver with the ADC32RF45. The ADC will be clocked at 3 GSPS, and Decimation mode will be set to divide-by-24 complex…
Hi Hariprasad
If you have the ADC12DJxx00 GUI installed (download from ADC12DJ3200EVM product folder), you can view the configuration files that are loaded. Registers are programmed in the exact sequence listed in each file. The files are located in…
Part Number: ADC32RF44EVM Other Parts Discussed in Thread: ADC32RF44 , LMX2582 , ADC32RF45 Hi,
We currently have ADC32RF44EVM attached to a KCU105 and have downloaded the KCU105 + ADC32RF44 Design Firmware from the TI website.
We have the ADC32RFXX…
Hi Satish
I am using the EVM GUI to configure the ADC and the LMK04828 and the LMX2582. Also i tried to use the Quick Start Button : But it didn't get the system running and the JESD204B synchronizing permanently. The EVM user guide also provides little…
Small correction from my original post. I realized that the LMK04828 data sheet includes a section on estimating the power consumption of a specific configuration and also found a spreadsheet calculator on another post. Using the spreadsheet and inserting…
Hi Jim,
I followed your recommendation. I have attached the log file. Seems all the writes are working well.
Fullscreen
log.txt
Download
Write Register: LMK04828.x000[0x0] -[0x80]
Write Register: LMK04828.x000[0x0] -[0x0]
Write…
Hi Taemin,
Yes, it is possible to change the sampling rate (1.5 to 3 GHz). Are you using the ADC32RF80EVM? There are some preset frequencies that can be generated by the onboard LMX2582. Additionally, you can use an external clock source (along with…
To elaborate, we have been building the LMX2594 EVM with 10 uF and that works fine, but 1 uF is the recommended value and that works. Note that from the sister part, LMX2582/92, 1 uF is both in the datasheet and the EVM.
Regards,
Dean