Thanks! Pls see follow-up question below.
Regards,
Jerome
Another question on these parts. Is there any difference between the LMZ21700 and the 701 besides output current rating?
Other Parts Discussed in Thread: LMZ21700
Hi,
I’m working in Japan disty , and now our customer would like to get 20 piceis of free sample of LMZ21700.
I tried to apply at the TI HP, but could not. Because the type name in question has not come…
The LMZ21700 does not need a Cff. The only requirement on the DS is Rfbb < 400kOhm. The same BOM should work fine for your Vout adjustable range. I think it should work well for your application.
regards,
Yang
The TPS62125 is not one of my products, but it looks like it should work. You may also want to look at the LMZ21700.
The input voltage range that we specify is the widest span that the regulator will function with. The actual input voltage range will…
Other Parts Discussed in Thread: LMZ20502 , LMZ20501 , LMZ21700 Does LMZ20502 start into Pre-Biased loads? If I switch quickly power on/off and output capacitors are still charged does it sink current or is there other problems (mayby broken circuit)…
All good inputs. As I've been told the TPS62179 is a replacement for the LMR22007. As another option I would also like to suggest using LMZ21700/01 for your entire requirement. These are the new nano modules and part of the SIMPLE SWITCHER family that…
Hi Arthur, If you give me your personal contact, I will send you our measurement results. Regarding OPA2188 I got an info that it contains PMOS only on it, so there isn't any crossover must be afraid of. I have 2 questions for you. 1. Reading your post…
The inductor on both of these modules is a non-shielded chip inductor.
I have attached the user guides for these devices; they include more EMI data.
The EMI testing was done on the EVM boards with the components specified.
Of course the EMI performance…