Hi Ki,
Attached you can find the 3 requested files. Note that I've changed the file ending to .txt because otherwise the forum wouldn't let me upload the files to this message. Unfortunately, no new crash dump file was generated during the crash. I…
Hi Todd,
Apologies. I thought I had added the link; somehow it didn't show up on here.
Here's the tutorial link:
TI_RTOS_Kernel_Workshop_Lab_Manual_rev4.00.pdf
I have also attached the lab manual of the tutorial. I am not sure if that helps…
Hello again John.
I tried but no chance... Now it opens with a blank black splash screen and after a couple minutes a different blank screen shows off. Like this:
Here are debug.txt and ccs_install_10.3.1.00004.log files:
0172.debug.txt
…
Hi George, thanks for answering.
I understand what you are saying but I'm not sure how I could fix it or even point exactly where the problem is in my project.
I have setup a very minimal project with a couple of lines of code and the result is…
Hi,
I installed v9.60.3 on my PC. And find this .dll file.
Please use it and try if it can work on your side. Change the .txt to .dll on your side.
armxds.txt
Best regards,
Cash Hao
Hi Rogelio,
thanks for the clarification about the supported commands. So, that seems to offer two options to go ahead:
1. Using the vendor specific commands to get WBS working also on CC2564C. In best case, we can keep our implementation compatible…
Hi all,
I am also facing the same issue with wl18xx on iMX6 Android Lollipop 5.0. Bluetooth bring up and scan remote devices with no issue. But transfer files to remote device would failed and system crash then reboot.
Please see attached log and…
Dear Ti E2E community
Am facing the clock drift issue when I run the below attached app, it says that sound card is facing clock drifts, but I don't see this issue in ti sdk 7, could you please try to reproduce this issue from your end & let me know…