Part Number: LP-CC2652RB Tool/software: Code Composer Studio I just received a LP-CC2652RB and am having issues in Code Composer.
I'm running Windows 10 as a development platform.
I've download and installed the more recent version of Code Composer…
Hi Nikolaj,
Thanks for the reply.
Nikolaj_G said: You mentioned that you have a 50-50 chance to flash the chip (see quote below). Does this mean that it does program the chip successfully some of the time?
Yes, at times it flashes the chip with…
Hi Piotr,
The command line tool does not parse or edit JSON files directly; this step would occur in the GUI tool. There is no " syscfg create_image" command in the CLI, as it does not have the dependency back to the SysConfig tool.
The FTDI or…
Hi TER,
Thank you for your reply. As I understand from your answer, it is possible for the CC1352P to be configured to run in external regulator mode described in Section 11.4 of User Guide.
I made an circuit to test this (VDDS_DCDC and DCDC_SW are…
Part Number: CC3235MODAS Other Parts Discussed in Thread: UNIFLASH Hi,
Further questions on designing a board to take either the CC3220MODAx or the CC3235MODAx module with antenna.
1. PCB Footprint : can you confirm the PCB footprint for both modules…
Part Number: LP-MSPM0L1306 Other Parts Discussed in Thread: MSPM0L1306 OS : Win 10
Browser : Chrome
OOBE URL : https://dev.ti.com/gallery/view/7473522/LP_MSPM0L1306_OOBE/ver/1.0.0/
Problem : With the Browser loaded with the Out of Box Example (OOBE…
I understand that I am able to program other MCUs using the eZ-FET on my LP. I am making multiple custom boards that each have a JTAG port for flashing to an MSP430. Because this is much faster than manually connecting header pins for each board, I prefer…
Hi,
Bootloader/Firmware on TiVa device (XDS110) might have corrupted or some Power supply issue. Did you check the PS Voltages on the Defective LP?
If the correct voltages are present nd still it doesn't show up then it might have a corrupted Bootloader…
Hi Shaoxing,
The typical usecase for the the LP-AM243 is assumed to be a desk/bench top where both the LaunchPad and the PC connected to the XDS110 are powered from the same source, sharing the same reference ground. In scenarios where the laptop or…
Part Number: LP-AM243 Hello,
I was working on the demo program " gpio_led_blink_am243x-lp_r5fss0-0_nortos_ti-arm-clang ". I was able to build the program with CCS11.
However, I was not able to load the program to the launchpad. I got Load program…