Part Number: LSF0002 Other Parts Discussed in Thread: SN74AXC2T45 , TXU0102 Tool/software: Hi Sir,
customer using LSF0002 for 70MHz signal but looks waveform abnormal when f>2MHz.
Do you have idea for this? thanks.
thanks, Ian.
Part Number: LSF0002 Other Parts Discussed in Thread: PCA9306 Tool/software: Hi team,
Could you please advise if LSF0002 could be used for VrefA=VrefB?
My customer VrefA=VrefB=1.8V. But the power rails are different. So, they want to separate by a…
Part Number: LSF0002 Tool/software: Hi team,
My customer is asking does we have extra ESD circuit in each pin.
I told customer our device has ESD protection (HBM and CDM). but they didn't see there is ESD circuit in our datasheet.
So they think…
Part Number: LSF0002 Other Parts Discussed in Thread: LSF0102 Tool/software: Hi, reading through the datasheet for the 1.8V to 1.2V bidirectional application, it's a bit confusing which side is A and which side is B for the reference voltage usage . Are…
Part Number: LSF0002 Other Parts Discussed in Thread: TXU0102 , TXU0202 Tool/software: Hi experts,
datasheet shows some schematics with pull- up resistor as following.
Could we change pull- up resistor to pull -down resistor?
If could, i s there…
Part Number: LSF0002 Tool/software: Hi,
Does TI have a 2-bit bidirectional buffer (push-pull) solution? <= Do not suggest the TXB series because it requires over 100Kohm pull-up resistors and cannot be used.
The speed should support over 10Mbps. …
Part Number: LSF0002 Other Parts Discussed in Thread: SN74AXC1T45 , SN74AVC1T45 , LSF-EVM , TXV0108 , TXV0106 , SN74AVC2T245 Tool/software: Hi,
I am looking for a way to converter a bi-directional signal with the left side being fixed at 1.8V and the…
Part Number: LSF0002 Other Parts Discussed in Thread: LSF-EVM , LSF0101 Tool/software: Is there an evaluation kit or IBIS model available yet for the LSF0002 part?
Part Number: TCA39306 Other Parts Discussed in Thread: LSF0002
Tool/software:
Hi, Im trying to make a switch and translator as shown in the below schematic.
During normal operation,
VIO_1V8 will be equal to VIO_1V8_PMIC. During production programming…