Other Parts Discussed in Thread: MSP430F47127 Hi,
I am producing my ac static energy meters based on MSP430F47127 for 3phase 4 wire network. Out of 100 meters 2-3 meters are stuck in field conditions. When we analysed these meters, we found that LF…
Part Number: MSP430F47127 I am making a energy meter/reference meter with 0.1 class accuracy based on MSP430F47127.
All thing is ok, but i am not able to provide pulse output for its accuracy check. Although i have provided 1600 impulse/Kwh output through…
Part Number: MSP430F47197 Other Parts Discussed in Thread: MSP430F47127 Dear All,
I am trying to set baud rate on MSP430F47127 and having problem.
Clock = 4194304
SCFI0 = FLLD_4+FN_4; SCFQCTL = 31; // (31+1) * 32768 * 4 = 4194304
I am trying…
Sir,
I am using fft routine for harmonics measurement for a 3 phase supply. And for that i use some calulations that require floating point values not the fft porgrams.
I first developed this code on a msp430f47127 using CCE. I changed my MCU to msp430f47177…
Aravind, The two microcontroller products that are included in the launchpad are these: * MSP430G2211IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT, BOR, Comparator A+ * MSP430G2231IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT,…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…