Part Number: OMAP-L138 Tool/software: I found that the CP15 registers were listed in \ccs\ccs_base\common\targetdb\Modules\CP15_ARM9.xml.
When I want to view a register,I must add the register's name to ccs->view->expressions.
How can I view all the…
Hello
I have assigned this to our DDR expert and also notified the folks who previously supported the SBL. This is now a legacy device , so support on it is limited. You may see some delay in response as it is a US holiday today and the fact that this…
Part Number: OMAP-L138
Tool/software:
Dear Sir/Madam,
Can i check where can i find the naming convention for OPAM-L138 family?
I would like to compare the real difference between OMAPL138EZWT3 vs OMAPL138EZWTA3, what does the A means?
To what…
Part Number: OMAP-L138 Tool/software: Hi,
I have an OMAP-L138 system with two flash memory chip: One on SPI1 that contains a program to check the other flash (SPI0) for two valid firmware versions.
The purpose of the two flash is to be able to always…
Part Number: DP83825I
Tool/software:
Hi, I configured my device tree to look like this, and I'm using the dp83825I phy chip, but I'm getting this error net eth0: could not connect to phy /soc@1c00000/mdio@224000/ethernet-phy@0
&mdio {
pinctrl…
Part Number: OMAP-L138 Tool/software: Hi,
How does the GPIO pins internally connected?
pull-up? pull down? 3-state?
What are the resistance values?
Thank you!
Richard Braun said: I'd appreciate if anyone here can confirm if a GOT indirection on top breaks the ABI or not, my understanding being that it does, but then I wonder why it was implemented that way.
The C6000 Embedded Application Binary Interface…
Part Number: OMAP-L138 Good Day,
I am having a problem writing the flash of a Omap-L138 custom board. I have a back up .bin that I would like to write to the nor flash to repair a firmware flash error that resulted in a non functional unit. I have been…
Part Number: OMAP-L138 Tool/software: Hello forum
Our company developed years ago a measuring device based on OMAP-L138 where the main system memory is a 8bit bus 1Gbit NAND flash. This system has a serial Flash to boot, and the used NAND flash is Micron…
Part Number: OMAP-L138 Dear TI,
because of CRA and NIS2 requirements, we are obliged to update the linux kernel to a recent version (continuesly).
I reckon that we are not the only ones who will have to comply with the upcoming EU-Regulation!
The…