Part Number: OPA197-Q1
Tool/software:
Hello TI,
Could you please provide information regarding output impedance/Resistance of OPA197-Q1.
Best Regards,
Manoj.
Part Number: OPA197-Q1 Other Parts Discussed in Thread: OPA197 , TINA-TI Tool/software: Hello TI,
could you please provide internal circuit block diagram for OPA197-Q1. I want to understand the device output behavior when there is a voltage present…
Part Number: OPA197-Q1 Dear Sirs
May I connect Pin_1 and Pin_2 on the OPA197-Q1? Does exist any limitation on the voltage that can be applied on Pin_1?
Thanks a lot again and best regards
Salvatore
Part Number: OPA197-Q1 Other Parts Discussed in Thread: OPA197 Tool/software: Hello TI,
I have a query regarding OPA197-Q1 output pin sink current during unpowered condition of the device. I could not find this information from the datasheet, however…
Part Number: TLV9151-Q1 Other Parts Discussed in Thread: OPA197-Q1 Tool/software: Hello Team,
I am using the TLV9151S op-amp in my project and encountering an issue. When the op-amp is disabled, I observe a voltage of 10 to 12 mV at its output pin.…
Part Number: TLE2037A-Q1 Other Parts Discussed in Thread: TLV197-Q1 , OPA197-Q1 , OPA192-Q1 , TLE2141-Q1 , OPA1612-Q1 Hello,
Good day, Customer wants a TLE2037a-Q1 pin to pin device within 1Mhz. Could you please give a recommandation. Thank you.
HI David,
The most similar device to the OPA191 (2.5-MHz) in automotive grade is the OPA2192-Q1 (10-MHz). The OPAx192-Q1 is a 36-V Precision, Rail-to-Rail Input/Output, Low-Offset Voltage, Low-Input Bias Current Op Amp With e-trim . The OPAx192-Q1 offset…
Part Number: ADS7887 Other Parts Discussed in Thread: OPA377-Q1 , OPA192-Q1 , TLV197-Q1 , OPA376-Q1 , OPA320-Q1 , OPA197-Q1 , OPA340 , OPA340-EP Hello,
I am trying to determine how closely the qualification test data matches with AEC-Q100 level screening…
Hi Daniel,
I forgot to list one important spec:
1. Automotive grade.
2. Slew rate higher than 4V/us.
3. MSOP8 package.
4. The V-/+ need to be higher than +/-20V.
OPA197-Q1 in only 18V.
Do you have other suggestion?
Many thanks.
Patr…
Yee,
So far we have been talking about the maximum input voltage offset of +/-100uV for a standard industrial part - OPA197. Having said that, the automotive grade of the part, OPA197-Q1, has the max offset at 25C of +/-250uV and up to +/-400uV over…