Part Number: OPA2188 Other Parts Discussed in Thread: ADS1262 , ADS1261 , ADS1248 , LM7705 , OPA2392 , LM4040 , ADS1118 , ADS1113 , ADS1115 , ADS1114 On the basis of OPA2188, I also carried out linearization according to the slyt442.pdf manual, LM 4040A…
Part Number: OPA2188 Other Parts Discussed in Thread: ADS1299 , , OPA2387 , OPA2388 , TLV2387 , OPA4387 , INA333 Tool/software: Hello,
We are currently in the process of designing the EEG data acquisition system using ADS1299, and we are considering…
Part Number: OPA2188
Hi team,
Could you help provide the data of OPA2188 below?
PART NAME
MAKER
Tamax
Tjmax
θjc(℃/W)
θja(℃/W)
θca
Pd max
Pdmax_fun =Pc
Pd-Ta waveform
Tamax…
Part Number: OPA2188-Q1 Other Parts Discussed in Thread: REF35 , , OPA350 Tool/software: Hi team.
my customer is developing a precision 16bit data acquisition system with using a SAR adc without refence buffer, can you help me on how to select a proper…
Part Number: OPA2188 Other Parts Discussed in Thread: OPA188
I have a question about Rail to Rail.
Perform the setup as shown in the figure.
Power supply voltage: 12V , Non-inverting input terminals: 3V
Measurement results:① Non-inverting input…
Part Number: OPA2188
Hi, Support Team
we saw the OPA2188 of datasheet 8.3.5 Electrical Overstress
about short duration is millisecond or microsecond level?
if any, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: OPA2188 Other Parts Discussed in Thread: TINA-TI There is a noninverting amplification circuit whose DC gain is 4.3. Due to the large and fixed output capacitor (C10: 10n~100n), the loop is not stable. The open loop bode is attached. besides…
Part Number: OPA2188 Other Parts Discussed in Thread: LM258 Hi Support team
my customer is asking if we have OPA2188 internal circuit like following from LM258
Part Number: OPA2188 Could you please tell me if the input stage of OPA2188 is FET or Bipolar?
Also, are there any common and general ways to distinguish these two kinds of stages?
Hi Raymond
I just found a package mistake of the BSS139H6327 on my PCBA. Just swap the gate and source,all is well and can limits the current low to 7mA under ± 60V.
Sorry I am not going to adopt the circuit you suggested,because it has lager PCB…