Part Number: OPA2994 Tool/software: I am using the OPA2994IDR and require a slew rate of at least 30V/µs. I am using the OP as an inverting amplifier with a factor of 1.5. Unfortunately, I am measuring a rise time of 20V/µs at the output.
I have seen…
Part Number: OPA2994 Tool/software: HI , see the sch , is it OPA2994 can work at vcc=12v and vee=-20v , input 2.4v , and want to get -2.4v*8.2=-19.68v , is it ok ? thanks.
Part Number: OPA2994 Other Parts Discussed in Thread: PSPICE-FOR-TI , TINA-TI Tool/software: I am using dual channel OPA2994IDGKR op amp. 1) I would like to know the exact current consumption when it is full load condition. How Can I calculate ? Please…
Part Number: OPA2994 Other Parts Discussed in Thread: OPA994 , , LM7321 Hi,
When will the OPA2994 / OPA994 be available to purchase from distributors (e.g. Digikey, Mouser)?
How can I order samples (OPA994 DBV Package, 5-Pin SOT-23). Will this part…
Part Number: OPA2994 Other Parts Discussed in Thread: OPA994 Tool/software: Hi team,
Just want to make sure, if the customer want to need op-amp to drive capacity load, is OPA2994 the best option? Their requirement is as below:
supply voltage: +/…
Part Number: LM6142 Other Parts Discussed in Thread: OPA2189 , OPA2994 Hi team,
we want to do p2p upgrade on LM6142BIMX/NOPB on customer side. Could you please kindly help provide comparison table between LM6142/ OPA2994/OPA2189 ? Thanks.
BRs
…
Part Number: ADS8638 Other Parts Discussed in Thread: LM358B , TLV2171 , OPA2994 , OPA140
Tool/software:
Hi All,
I have a question about ADS8638. I understand that 1200pF is installed to suppress glitches, but the capacitance seems a little large…
Part Number: OPA994 Other Parts Discussed in Thread: OPA2994 Tool/software: Hi
According to Figure 5-49 Short-Circuit Current vs Temperature, does the curve imply that the user can short the output to GND continuously?
My application condition is…
Part Number: LM7322 Other Parts Discussed in Thread: OPA2994 Sir
We are planning to use the LM7322 to drive a MOSFET.
The operation condition is listed as follows
VS = + - 15V (Dual power supply)
VO = VGS = 2 ~ 3V
MOSFET = AOD496, Ciss = 1200pF_Max…
Part Number: TLV2474 Other Parts Discussed in Thread: OPA994 , OPA2994 Tool/software: Hi ,
We are using the TLV2474 quad OP AMP as a voltage follower to drive reference voltages to digital trim pots. Currently the design operates at +3.3V and buffers…