Part Number: OPA3695 Tool/software: Dear Team,
I am designing a signal conditioning circuit for offset and gain adjustments referring to TI's doc . I have to amplify my sine wave from ±0.5V to 0 -3.3V. the signal frequency maximum is 100MHz. I selected…
Other Parts Discussed in Thread: OPA3695 Hi!
I need high speed amplifiers with high slew rate in order to amplify a differential signal coming from sensors. In the end I need a single signal so I figured the best option is to use the OPA3695 since…
Part Number: OPA847 Other Parts Discussed in Thread: THS3491 , OPA695 , LMH6702 , OPA3695 Dear Sir or Madam,
I would like to use the OPA847 in non-inverting configuration at a gain of 2. Is there a recommended external compensation circuit for this…
Part Number: LMH6733 Other Parts Discussed in Thread: LMH6738 , OPA3691 , OPA3695 Hi Expert,
LMH6733 and LMH6738 are pin to pin solution, but could you also help to confirm if these two parts are BOM to BOM compatible solution ?
Regards,
Mark
Hello Jorn,
Instead of using the LMH6702 to create a differential driver for the ADC12D1800 ADC, it might better if you looked at the Fully Differential Amplifiers (FDA) instead. TI has a portfolio of these devices:
http://www.ti.com/paramsearch/docs…
Kaspars,
None of the devices I listed come in quads. The OPA695 has a dual OPA2695 and a triple OPA3695. The THS3201 has a dual THS3202. The THS3091 has dual THS3092.
The THS6002 and THS6184 are quad CFB amps that are designed for dual por DSL line…
Other Parts Discussed in Thread: THS7360 , OPA3695 Dear all,
Recently, I encounter a signal quality issue about Analog RGB signal.
I measure the VESA spec. The spec of rise/fall time is 1.66ns if resolution is 1080P 60Hz.
If you want to achieve…
Other Parts Discussed in Thread: THS7347 , THS7327 , THS7353 , TVP7002 , THS7303 , THS7368 , THS7364 , OPA3690 , OPA3693 , OPA3695 , OPA2830 , SN10502 , SN10501 Hello,
Can anybody please tell me of an alternative to THS7347/ THS7327 buffers. Actually…