Part Number: OPA377 Hi,
We use OPA377 to build a thermal couple signal amplifier as showed below:
This application has been using for a long time. With a constant input, the output has recently been showing random results at each power-up. The…
Part Number: OPA377-Q1 Other Parts Discussed in Thread: TLV9051-Q1 Tool/software: Hi, I'm generating a quotation for a large automotive OEM who require manufacturing information to be able to accept our quote; fab plants, technologies etc.
Where should…
Part Number: OPA377 Tool/software: Our production line is impacted by a problem, which fail rate suddenly increased higher recently.
After team analysis, we suspected that the component HM39100237(MPN: OPA377QDBVRQ1) is related to this problem.
…
Part Number: OPA377 Other Parts Discussed in Thread: TINA-TI Dear Sir:
Regarding the OPA377 Power OFF PIN internal Status
When the OPA377 Power OFF(no power supply).
*Which the following the Pin internal status of +IN(Pin1) at OPA377 Power OFF …
Part Number: OPA377-Q1 Other Parts Discussed in Thread: OPA377 Hi Team,
As i am working on amplifier OPA377QDBVRQ1 and require some input
1. output voltage V/s output current graph at 85degC for 0 to 3.3V
In datasheet it provide -40 to 150 degC
Hi Sean,
I am unable to comment on your plot, but I can try to explain the numbers below. If you still have the question, please post the schematic.
0.117489755493953 2.0935011595101E-7 3.71340625965945E-5
0.117489755493953 means the frequecy is…
Part Number: OPA377-Q1 Other Parts Discussed in Thread: OPA377 I use the OPA377 as a current limiting circuit.
The voltage of the 3 pin of OPA377 is 0.19V,but the voltage of the 4 pin of OPA377 is 0.72V。
The voltage of the 3 pin and the 4 pin should…
Part Number: OPA377-Q1
Hi, this for MPN-OPA377QDBVRQ1. In the above circuit to find out the voltage at negative terminal (V.NEG) what are the voltages need to be considered considering all offset. If you can provide the equations for V.NEG it would…
Part Number: OPA377 Hi team,
My customer has a SPK AMP (TPA2010) design, the line out of the CPU and the line out of the codec are simultaneously connected to the SPK AMP (TPA2010) through the Pre-AMP (OPA377).
Two line outs may be output for mixing…
Alberto,
You are correct, the influence of offset voltage in your non-inverting amplifier is the same as the gain equation for the circuit. It's relatively easy to see its influence in this circuit since the offset voltage is added directly in series…