Part Number: OPA4872-EP Tool/software: Hello,
As per datasheet OPA4872-EP it is mentioned that operating supply voltage is +/-5V.
Is this device operating with unipolar voltage 0 to 5V?
Input at mux would be 0 to 3.3V.
Thanks,
Nilesh Kara…
Jacob
Thankyou for the reply. I was on medical leave so couldn't reply you earlier.
There is a part b of above question.
As a microcontroller is running with DGND reference and analog signals are runnning with AGND reference, and to use OPA4872…
Part Number: OPA4872-EP Other Parts Discussed in Thread: OPA4872 Hi
I'm using three OPA4872 as 8*1 multiplexer. What is the propagation delay of one channel of a multiplexer?
Regards;
Part Number: OPA4872 Other Parts Discussed in Thread: OPA4172 , OPA695 , Dear Sir/Madam,
I need a 10:1 mux that supports from 0Hz to 200MHz. I am wondering if it is a good idea to cascade as shown below and whether I need an additional op amp to drive…
Other Parts Discussed in Thread: OPA4872 , TINA-TI Hello,
I need the propagation delay of "OPA4872MDREP", but I can't find in datasheet.
Can you please help me out to find this?
Part Number: OPA4872-EP Other Parts Discussed in Thread: OPA4872 Hi
I intend to use OPA4872-ep as a video multiplexer as a replacement of Max440. Is it recommended for video multiplexer? From the spec it looks that it can be used as a video multiplexer…
Other Parts Discussed in Thread: OPA4872 Hello,
My questions concern the OPA4872. I would like to use this component for 4:1 composite video multiplexing, however, I am new to the field of circuit building and am not familiar with all of the OPA4872…