Part Number: OPA836 Other Parts Discussed in Thread: OPA838 , , OPA837 Hi team,
My customer is using our OPA836 & OPA838 now.
And they wonder if we have a newer device to recommend.
Requirements:
BW: >200MHz
slew rate:>200V/us
Iq:<1mA
…
Part Number: OPA836 Other Parts Discussed in Thread: THS3217 , THS3491 Long time ago (2005) I had put together this AN135 application note, at the time there was a excel spreadsheet that went with it. Two questions -
https://www.ti.com/lit/an/sbaa135a…
Part Number: OPA836 I want to use OPA836IRUNT as a non-inverting amplifier with a gain of +1. I shorted Output (pin1) and inverting input (pin 2). What I should do with pin 6,7,8,9? Can I leave open these pins?
Hi,
why have you chosen the OPA836? Because of the low supply current?
Why have you chosen figure 60 as reference? Your input signal is not swinging arround a bias voltage of 2.5V.
Why must the input impedance be 1M? In this case you should look…
Part Number: OPA836 Other Parts Discussed in Thread: TINA-TI Hi Team,
i was reading our datasheet today but have some confusion with datasheet.
1. when used split power supply with both postive and negative power supply, how to push the OPA836 to…
Part Number: OPA836 Hi team,
According to OPA836 PDS: "To protect the input stage of the amplifier, the devices use internal, back-to-back ESD diodes between the inverting and noninverting input pins.", we can see there are diode between Vin+ and Vin…
Hi David,
Please see the output swing mentioned in the datasheet table data for OPA836.
So depending on the swing, the lower side output is not supposed to reach 0V or the negative supply based on DS(and as implemented in the model)
Can you…
Part Number: OPA836 Hello,
Is there a matching spec for the integrated resistors? I understand that they are laser trimmed to +/- 1% accuracy, but want to confirm is the ratiometric matching is better than 1%.
Don
Part Number: OPA836 Other Parts Discussed in Thread: OPA837 , OPA2834 , OPA197 Hi team,
My customer is evaluating OPA836 in a water meter project. This project cares about the power consumption very much. Customer found OPA836's Ib is as below:
…