Part Number: TDA4VM Other Parts Discussed in Thread: TDA4VL Hi TI experts,
Custom tda4vm-echo board & SDK (PROCESSOR-SDK-RTOS-J721S2 08_00_04_04 )
Issue: R5F DSI Display Not works. There is no output from dsi mipi-data pins.
my board is designed…
To be clear, I attached log text files written on when reboot fail and success.
According to the logs, the log stop while it is written after around 7 seconds. I observe every reboot failure this after few hours with similar log when reboot fail.
…
Hi Jack, Yes, the secure SDK 6.3 prebuilt images boots ok on AM437x HS EVM. I'm attaching the log file for your reference. Best, -Hong
Fullscreen
am4_6.3_hs_boot.txt
Download
U-Boot SPL 2019.01-g333c3e72d3 (Apr 19 2020 - 03:04:54 +0000…
SI,
Please see the attached presentation. It was originally prepared for the LM10010 which was later superceded by the LM10011 which has higher precision. Please also see the many E2E posts discussing the LM10011 and TPS56121 with C667x and C665x. …
Hi Please find the log file Linux log -
Fullscreen
uart_2_linux_log.txt
Download
Welcome to minicom 2.8
OPTIONS: I18n
Port /dev/ttyUSB2, 10:46:48
Press CTRL-A Z for help on special keys
U-Boot SPL 2023.04-ti-gf9b966c67473 (Mar…
Hi, there:
TI radar device can support CW mode, but the SDK OOB demo does no support this mode and we do not have application demos for CW mode. I would suggest you to go through ICD document to find the CW mode related API /cfs-file/__key/communityserver…
Hello Schuyler,
I think source file dp83tc817.c have some issue beacuse the function " dp83tc817_config_init " is used to read and write 0x0608 offset register. But the 0x0608 is a indirect access register. here in source file try to read directly…
Hi Bin,
I've tried this prebuild image with exactly the same results.
Please see attached the boot log
.
U-Boot SPL 2021.01-g44a87e3ab8 (May 14 2022 - 22:32:40 +0000)
Trying to boot from MMC1
U-Boot 2021.01-g44a87e3ab8 (May 14 2022 - 22…