Sir,
we have set the CUV Threshold:3500mv recovery :3800mv. but when we have connected the load and started discharging the battery pack, even when one of the cell voltages is dropped to 2600mv ,FETs are not turned OFF . and the system is not going…
Hi Michel,
One further question please?
On page 2-3 of the Network Processor Interface User's Guide (attached below). Its says that the 1310 does not support hardware flow control, CTS and RTS.
I currently have an FTDI cable (USB to Serial cable…
Hi Vivek,
Thank you for the response. So, How will the initialization on WDT be? I did not find any info on the reference manual too.
How do I link Watchdog to NMI handler?
spruh22h.pdf
Yes, you have per rail Vout, Iout, and Temp scale and offset control via the Other Config tab. And, as you've mentioned the exponent allows you to tune the resolution and upper voltage limit.
Also, I've attached an "in work" app note which describes…
Part Number: BQ40Z50-R1
Hi
The customer design with BQ40Z50-R1, the battery fail return from the end user because the fuse broken. FUSE_EN,PTC was disable.
Products placed in warehouse also have been found the fuse broken. The screen as below. …
Hi,
I had lunched same test application "Myapplication4.rar" on aosp 08_03 and 08_05.
The 08_05 result is no better than 08_03.
I had provided logcat log and delay time experiment log.
Fullscreen
android_08_03 experiment log.txt …
As I said, I am experimenting or trying to familiarise myself with CSS and EK-TM4C1294XL.
I took the last step ( the Widget example) from lab16
and changed the Lab04 of (TI_RTOS_Kernel_Workshop_Lab_Manual_rev4.00.pdf) TI_RTOS_Kernel_Workshop_Lab_Manual_rev4…
Other Parts Discussed in Thread: TVP5150AM1 Hi,
We have Appro IPNC kit with DMVA2. The original kit came with MT9P031 sensor which we have replaced with custom TVP5150AM1 deocder board. We have done the following configurations:
DECODER :- The decoder…