Hello Villegas,
*********Are you using a XIO2200 Evaluation module?
we used our board which i copied from XIO2200 Evaluation module. We test the board PC. it succesfully write EEPROM using Ohcirom.
********Do you have series capacitors on…
Other Parts Discussed in Thread: TMP112 Hi,
We designed video processing board based on TI DM8168 . We are trying to capture 576i SD video which is streaming over Ethernet , while doing this task we encountered with below error very frequently, please…
Other Parts Discussed in Thread: BQ20Z45 Dear Sir,
We would like to inquire regarding the INIT bit for BQ20Z45
Our customer has asked us to simulate our battery pack with high discharge power (178W) under high ambient temperature (60degC). For this…
Hi Andy,
Thank you for the response.
I initially had the charge term voltage set to 10mV but recently lowered it to 1mV during trial and error testing. I increased it to 50mV and retested last night but the results were the same. Here is the updated…
Other Parts Discussed in Thread: CCSTUDIO I encountered some problem on compiling the psp example-- C:\dvsdk_1_11_00_00\pspdrivers_1_10_00\packages\ti\sdo\pspdrivers\system\dm6437\bios\evmDM6437\i2c\build\dm6437_evm_i2c_st_sample.pjt
when I open " dm6437_evm_i2c_st_sample…
I tried creating the platform in the bios... directory, but under "myplatforms". I couldnt' get that to build. (Lots of Java whines.) I moved the whole thing into ti/platforms, and it built fine. (Yes, I had added the directory to the dsp builder tab…
Part of the device address (bit 0) is a read/write bit. The device address is 0x16. Depends on if it is a read/write, the device address change between 0x16 and 0x17.
Basically, you will send 0x17 as the device address after re-start in SMBus read…
Yass,
Which GEL file are you using? I think you may need an updated GEL file which configures the USB hardware properly. I was able to get the usbhostmsc example working with this GEL file update.
Please try out the following GEL file with your setup…
It is a bit unclear from your description, what you are trying to debug and what component source code you are trying to step into so let me get some clarification and provide you guidance based on my understanding of your debug.
You have a custom board…
Jeff,
I think the 0x0010 0000 on page 97 of spru612d is a typo and should be 0x0020 0000.
Jeff Brower said: Question 1 -- when we use 0x0020 0000, is this working because it's a 'reflection' of 0x0010 0000?
Is the same data available if you move…