Hi,
1) Are you sure you want to have access to the PDM data? In general, the useful data are the PCM data.
To get the PCM data it is quite easy: you basically need to use the function PDMCC26XX_requestBuffer() as it is done in the SA_processPDMData…
Hi Khalefa,
I just tried SLS example using the UART interface with a CC3100 module and it worked fine without any issue.
Few points/questions:
Are you using the simplelink studio example provided in SDK? I hope you are defining ' SL_IF_TYPE_UAR…
Part Number: CC3220SF-LAUNCHXL Other Parts Discussed in Thread: UNIFLASH , CC3220SF I've been working with the CC3220SF-LAUNCHXL and I can't get the UniFlash program to connect to it. I was going step-by-step through the 'UniFlash ImageCreator Basics…
Hi Praneet
I'm using a MSP430G2955 host. No, I don't use the Simplelink Studio. I'm using the Code Composer Studio (Eclipse).
This protocol error happens on every device we have. But it's quite hard to reproduce (~ once in 4h).
It happens with the…
Part Number: CC2640 Other Parts Discussed in Thread: CC3200 , CC3100 , CC1310 , CC2650 , SYSBIOS General TI-RTOS changes
TI-RTOS drivers and board files have moved to a new TI-DRIVERS component. Refer to the TI-DRIVERS section below for more details…
Hi Ralph,
That is the issue I believe. You need to remove any existing image from the external serial flash in order for this to work. If the network terminal example is still on there it will boot. If the valid image is removed, the debug header will…
Other Parts Discussed in Thread: CC3200-LAUNCHXL , CC3200 A bit of information about my setup
Service Pack 1.0.0.1.1
CC3200-LaunchXL v3.2
CCS v6.0.1.40
CC3200 SDK V 1.0.0
I've been having intermittent issues with the CC3200 code crashing every…
Part Number: LP-CC2652RB Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1 , SYSBIOS , CC2650 Hi
I've been experimenting with the project zero example from the SimpleLink CC13x2 26x2 SDK (Version 5.20.00.52) on the LAUNCHXL-CC26X2R1 launchpad with…
Part Number: CC2642R Other Parts Discussed in Thread: CC2640R2F , CC2640 , CC1350 , CC1310 , CC2650 , SYSCONFIG
Note: The following instructions have been written for SDK 3_40_00_02 but can be adapted to quite any SDK version (that is why I provided…