Hi Walter,
I am not too familiar with the PIC18F258 microcontroller but I believe there is only one CAN controller built in. You mention connecting 3 transceivers. Are you planning on having 3 PIC microcontrollers and 3 external CAN transceivers?
…
Hello Ninand,
SN65HVD251 should be OK. Note that SN65HVD1050 is a High Reliability part. Also do make sure that the specifications meet your requirements irrespective of which part you select.
Regards
Amit
Hi Akhil,
Why there is a different voltage between 'All pins' and 'CANH, CANL and GND' above?
Typically on devices like transceivers the bus pins will include additional ESD protection since ESD event most commonly occur on the bus. There is a typo…
Also note the SN65HVDA1040-Q1: http://focus.ti.com/docs/prod/folders/print/sn65hvd1040-q1.html , the SN65HVD251: http://focus.ti.com/docs/prod/folders/print/sn65hvd251.html , and the SN65HVDA541-Q1: http://www.ti.com/product/sn65hvd251 also support J1939…
Part Number: TCAN1042HG Other Parts Discussed in Thread: SN65HVD230 , SN65HVD251-Q1 Dear Team,
Do we have CAN device without time out function?
The customer don't want the CAN device have time out function
BR
Kevin
Other Parts Discussed in Thread: SN65HVD251 , SN65HVD255 , HVDA551-Q1 , HVDA553-Q1 Hi,
I'm currently working with the SN65HVD251 as a CAN transceiver to output J1939 frames. I'm revising the design and I came across the new SN65HVD255 supporting the…
Other Parts Discussed in Thread: SN65HVD252 , SN65HVD251 Hello,
Q1. Do you have a specification about receiver input pulse width on SN65HVD252?
Q2. Is there any hardware difference between SN65HVD252 and SN65HVD251 concerning receiver input pulse…
Other Parts Discussed in Thread: SN65HVD1050 , SN65HVD251 , SN65HVDA1050A-Q1 , SN65HVDA542-5-Q1 , SN65HVDA1040A-Q1 For a better EMC peformance we wanted to change to the CAN Transceiver SN65HVD1050. But a start up test at about -25C showed that the CAN…