Part Number: SN74AUP1T50 Other Parts Discussed in Thread: SN74AUP1T17 , Hello, Can you, please, indicate the main differences between SN74AUP1T50 and SN74AUP1T17 devices? Thank you, Jose
Part Number: SN74AUP1T17 Other Parts Discussed in Thread: SN74AUP1T50 What is the difference between these two part numbers? They seem identical.
Thanks
Part Number: SN74AUP1T50 I am trying to find a replacement for a 1T34 unidirectional voltage translator that is out of stock (currently using OnSemi NLSV1T34DFT2G). I am trying to buffer a +3.3V signal entering my board before it enters an FPGA. Although…
Part Number: SN74AUP1T50 Other Parts Discussed in Thread: SN74AUP1G17 Dear team,
As topic, may I know if SN74AUP1T50 can be used in 3.3V to 1.8V system? If yes, what is Vcc that we should use? Thank you.
Regards,
Polly Chung
Other Parts Discussed in Thread: SN74AUP1T50 I have designed the SN74AUP1T50 into my system and have since found that the Tpd spec falls outside of my application. But, I only need a temp range of 0C to 45C with a 10pF load. Do you have any Tpd data for…
Other Parts Discussed in Thread: SN74AUP1T50 , SN74AVC24T245 Hi sir,
I want to find a product in TI catalog.
-Transfer 1.8V to 3.3V
-frequency 20~50MHz
-square wave signal
-22 channels.
BTW, can I use SN74AUP1T50 on single channel to transfer…
Part Number: SN74LVC1G17 Other Parts Discussed in Thread: SN74AXC1T45 , 2N7001T , SN74AUP1T50 , SN74AUP1T34 , TXU0101 , SN74AUP1T17 hi teams:
1. The trigger level of sn74lvc1g17 is 1.48-1.92v. Can it be confirmed that 1.8V can be triggered 100%,
Whether…
Part Number: SN74LVC1404 Other Parts Discussed in Thread: SN74AUP1T50 Hi all,
Below is the schamtic, when all three outputs are used, high level volatage of OSCIN_24MHz is 1.27V , AEC_24MHZ is 1.2V,HDMI_I2S2_MCLK is 0.65V, (clock high level minimum…
Other Parts Discussed in Thread: TRS3221 , SN74AUP1T50 Hi,
I am using the TRS3221 in a UART application (PC -> DB9 -> TRS3221). The logic level for my device is 2.5V (3.3V input tolerant) therefore I am using a level shifter, SN74AUP1T50, only on DIN…