Hi Tim,
Sorry , yes , I meant the SN74AVC2T872 device.
The LSF is a generic level shifting device for voltage translation through pullup resistors, the speed limited by the R pullup and the output load capacitance.
The TXS architecture has the…
Please refer to the FAQ on the recommendations based on the interface being used:
Also included the questions before we can recommend the right device:
Questions_Level translation.pptx
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Here are the voltage level translation device recommendations for various industry standard interfaces:
Interface
Recommended Device
3.6V Maximum
5.5V Maximum…
Hi Abhi,
In terms of the operation, this device is application specific to MMC. But, we understand that there are various requirements as the standards evolve.
I have attached a ppt which could be useful for us and hopefully for you to evaluate the…
Hello,
Did you come across any direction-sensing circuit?
Is SN74AVC2T872 the sensing IC that what my customer is looking at?
I come across an applicaiton notes from NS at per attached.
Can I check do we have any application notes on this…
Quickly find solutions to common questions about voltage translation (level shifter) devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
Auto-Bidirectional Level-Shifters
Fixed DIR / DIR…