Part Number: SN74AXC4T774 Tool/software: Hi
If input signal slew rate is 5V/ns then what will be output slew rate when translating down as below with 100 MHz frequency.
Case1: 3.3V to 0.8V (A to B)
Case2: 3.3V to 2.5V (A to B)
Will it keep maintain…
Part Number: SN74AXC4T774 Tool/software: Hi,
We are looking this device for Test (ATE) applications where different data protocols (as SPI, JTAG etc.) are running.
One side (VCCA) we will have fixed Input signal voltage as 3.3V and another side (VCCB…
Part Number: SN74AXC4T774 Tool/software: We are currently evaluating the SN74AXC4T774 for use in one of our designs and would like to simulate its behavior in our circuit environment. However, we were unable to locate a SPICE model for this device on…
Part Number: SN74AXC4T774 Tool/software: Hi Team,
I noticed a significant leakage current on the P_VDDH rail when the level shifters are enabled by pulling the EN pin low.
We have two level shifters onboard, and each draws approximately 160 mA, resulting…
Part Number: SN74AXC4T774-Q1
Tool/software:
Hi Team,
Using the level shifter, we are simulating an SPI interface which translates from 3.3V to 1.8V. @20Mhz
The waveforms at the output of Level shifter seems to be improper.
The signal low seems…
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: TXB0104-Q1 Tool/software: Hi team,
Can you please review the CAXC4T774QBQBRQ1 SCH as below?
BTW, can CAXC4T774QBQBRQ1 support 20MHz SPI interface? Thanks
Best Regards,
Xiaowei…
Part Number: SN74AXC4T774 Tool/software: The site says that SN74AXC is the newer/upgraded version of SN74AVC for SN74AXC , the datasheet states there are integrated 71Kohm pull-down resistors on the I/Os, so "if an external Pull-Up is required, it should…
Part Number: SN74AXC4T774 Other Parts Discussed in Thread: TXV0106 Tool/software: I am currently using the CAXC4T774QRSVRQ1 for level translation between VCCA of 1.5V and VCCB of 1.8V which appears to be a family part of the SN74AXC4T774. The interface…
Part Number: SN74AXC4T774 Other Parts Discussed in Thread: TXB0304 , TXV0108 Tool/software: Dear team,
I see in D/S sn74axc4t774 mentioned the max data rate is 320MHz with 3.3 V to 1.8V, but how about 1.8V to 1.2V? for Quad SPI the max data rate will…