Part Number: SN74LVC16T245 Dear Team,
Could you please tell me Input pin max current at operation?
Does it depend on the output pin current?
Best Regards,
Seijiro Matsuoka
Part Number: SN74LVC16T245-EP Tool/software: Hi,
Please specify the maximum data rate of the CLVC16T245MDGGREP and whether it supports SPI.
Thanks and Regards,
Annapoorneshwari M K
Part Number: SN74LVC16T245 Looking for recommended operating junction temperature rating of device. Absolute max (150C) is specified as well as ambient (85C).
Would recommended junction temperature be 125C? If so, would you be able to include this…
Part Number: SN74LVC16T245 Tool/software: Hi,
Iam using (SN74LVC16T245) Part for Level Translation Application, In my case VCCB is Fixed & that IO Signals are 3.3V , VCCA Port Signals Can be 1.8V or 2.5V or 3.3V or 5V but Present it will be 3.3V IO…
Part Number: SN74LVC16T245 Tool/software: Hi all,
I would like to confirm about ''10.1.1'' .The usage conditions are Vcca=3.3 V, Vccb=5 V.
It is defined as below, but where are the propagation delays (DIR to A) and (DIR to B) defined?
I saw the…
Part Number: SN74LVC16T245 Tool/software: Hello,
I have a question about this SN74LVC16T245DGGR integrated circuit.
I have the integrated circuit on a PCB, and I would like to know if it is possible to change the inputs and outputs whenever I want…
Part Number: SN74LVC16T245 Tool/software: Hi,
I am using this part " CLVC16T245MDGGREP " as buffer operating at 1.8V (VCCA=VCCB=1.8V), Not as level translator.
I want to know what is the maximum data rate supported by " CLVC16T245MDGGREP" IC with…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74AVCA164245 Tool/software: Dear Sir/Madam, We are planning to use 16-bit Buffer IC SN74LVC16T245DGGR in our design as a replacement for AVC part (PI74AVC164245AE). Kindly find the following…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74ABT162245 , Tool/software: I have SN74LVC16T245 with 3.3V supply voltage and the I/Os are connected to the I/Os of SN74ABT162825 and SN74ABT162245 with 5V supply voltage. The VIH, VIL, VOH…
Part Number: SN74LVC16T245 Tool/software: Hi team,
In the datasheet, it is described that there is BGA package type (GQL/ZQL).
Is this still active? I cannot find in TI.com.
Best regards, Goto